2013-09-20 11:30 PM
I'm using stm32f4discovery-BB board andTFT LCD (SSD2119 LCD driver) from Embest technology, I've ported all themodules on the Discovery with the help of the STemWin example on stm324xG-Evalboard as far as I understood. But now the display goes on blinking continuouslywhenever I run my program. Can someone suggest me what could be the problems Ineed to look back again???
Also I couldn't make out why in the givenexample FSMC Bank 1 NOR/SRAM2 in initialised in SRAM_Init() while in actualparrarel interface for the LCD occurs in FSMC Bank 1 NOR/SRAM3...Please someonegive some clue. I'm trying out all sorts of modifications but unable figure outthe root of the problem. Something I must be missing.
2014-01-22 8:18 PM
I am also trying to use emWin demo with keil on stm32f4dis-BB. Is there anyone can share the working demo to me, my email is: kqian@atcinc.net. Very thankful for that.
2014-02-14 11:55 AM
I'm trying to use emWin demo with stm32F4 Discovery and SS2119. Is there anyone can share the working demo with me? my email is: daniel.casini@gmail.com
Thanks,Daniel2014-03-22 8:25 AM
2014-03-22 6:54 PM
''Share'' is a two-way street - recent posts are primarily, ''give'' only.
Requesting private response (via personal email) defeats the general learning process of the forum - not exactly forum's purpose/intent... And - ''expecting'' a reply is especially offensive...2014-03-22 8:20 PM
I wait hopefully for my share of hardware, and treasure...
2014-03-24 12:08 AM
While your ''new image'' is distinctive/sophisticated - it deviates from my image recall during our seminar meeting - thus intrudes into quick/eased transfer of, ''hardware/treasure.'' (which you've so clearly - earned...)
2014-03-30 10:03 AM
Thank you to toth.janos after scratching my head i had created driver exactly like you ... but then Config.RegEntryMode = 0x6830; was missing..
After looking to comment of sen.tapabrata I looked in to my data sheet of SSD2119 for R11h Reg n it worked with correct address of Config.RegEntryMode = 0x6230; Thank you for this post guys..2014-06-26 7:35 AM
Dear Sir,
For my first post, I'll try to be complete. I had some difficulties to get here, but now I have only one problem. Your comments have been of great help.The screen displays the correct image, but with a red tone. I probably forgot something, but I can not find. The problem must come from a misconfigured setting.Hoping to find quickly, I will post my solution if I find it. Thank you in advance.2014-06-27 5:41 AM
Well, I found my error:
I had to change this:pDevice GUI_DEVICE_CreateAndLink = (GUIDRV_FLEXCOLOR, GUICC_565, 0, 0);
/ / = pDevice GUI_DEVICE_CreateAndLink (GUIDRV_FLEXCOLOR, GUICC_M565, 0, 0);
Thank you again for the information that helped me to get here.
2018-04-26 2:52 AM
I'm looking for a working demo of STemWin using Keil 5 on stm32F4 Discovery (stm32F4 discovery BB board and TFT LCD) LCD controller SSD2119. Can anyone, please, share his demo with me ? my email :
mailto:amridhafer10@gmail.com