2024-07-12 03:21 AM
in stdlib version1.9.0,
void I2S_Init(SPI_TypeDef* SPIx, I2S_InitTypeDef* I2S_InitStruct)
{
uint16_t tmpreg = 0, i2sdiv = 2, i2sodd = 0, packetlength = 1;
uint32_t tmp = 0, i2sclk = 0;
#ifndef I2S_EXTERNAL_CLOCK_VAL
uint32_t pllm = 0, plln = 0, pllr = 0;
#endif /* I2S_EXTERNAL_CLOCK_VAL */
/* Check the I2S parameters */
assert_param(IS_SPI_23_PERIPH(SPIx));
assert_param(IS_I2S_MODE(I2S_InitStruct->I2S_Mode));
assert_param(IS_I2S_STANDARD(I2S_InitStruct->I2S_Standard));
assert_param(IS_I2S_DATA_FORMAT(I2S_InitStruct->I2S_DataFormat));
assert_param(IS_I2S_MCLK_OUTPUT(I2S_InitStruct->I2S_MCLKOutput));
assert_param(IS_I2S_AUDIO_FREQ(I2S_InitStruct->I2S_AudioFreq));
assert_param(IS_I2S_CPOL(I2S_InitStruct->I2S_CPOL));
/*----------------------- SPIx I2SCFGR & I2SPR Configuration -----------------*/
/* Clear I2SMOD, I2SE, I2SCFG, PCMSYNC, I2SSTD, CKPOL, DATLEN and CHLEN bits */
SPIx->I2SCFGR &= I2SCFGR_CLEAR_MASK;
SPIx->I2SPR = 0x0002;
/* Get the I2SCFGR register value */
tmpreg = SPIx->I2SCFGR;
/* If the default value has to be written, reinitialize i2sdiv and i2sodd*/
if(I2S_InitStruct->I2S_AudioFreq == I2S_AudioFreq_Default)
{
i2sodd = (uint16_t)0;
i2sdiv = (uint16_t)2;
}
/* If the requested audio frequency is not the default, compute the prescaler */
else
{
/* Check the frame length (For the Prescaler computing) *******************/
if(I2S_InitStruct->I2S_DataFormat == I2S_DataFormat_16b)
{
/* Packet length is 16 bits */
packetlength = 16;
}
else
{
/* Packet length is 32 bits */
packetlength = 32;
}
if(I2S_InitStruct->I2S_Standard <= I2S_Standard_LSB)
{
/* In I2S standard packet length is multiplied by 2 */
packetlength = packetlength * 2;
}
/* Get I2S source Clock frequency ****************************************/
/* If an external I2S clock has to be used, this define should be set
in the project configuration or in the stm32f4xx_conf.h file */
#ifdef I2S_EXTERNAL_CLOCK_VAL
/* Set external clock as I2S clock source */
if ((RCC->CFGR & RCC_CFGR_I2SSRC) == 0)
{
RCC->CFGR |= (uint32_t)RCC_CFGR_I2SSRC;
}
/* Set the I2S clock to the external clock value */
i2sclk = I2S_EXTERNAL_CLOCK_VAL;
#else /* There is no define for External I2S clock source */
/* Set PLLI2S as I2S clock source */
if ((RCC->CFGR & RCC_CFGR_I2SSRC) != 0)
{
RCC->CFGR &= ~(uint32_t)RCC_CFGR_I2SSRC;
}
/* Get the PLLI2SN value */
plln = (uint32_t)(((RCC->PLLI2SCFGR & RCC_PLLI2SCFGR_PLLI2SN) >> 6) & \
(RCC_PLLI2SCFGR_PLLI2SN >> 6));
/* Get the PLLI2SR value */
pllr = (uint32_t)(((RCC->PLLI2SCFGR & RCC_PLLI2SCFGR_PLLI2SR) >> 28) & \
(RCC_PLLI2SCFGR_PLLI2SR >> 28));
/* Get the PLLM value */
pllm = (uint32_t)(RCC->PLLCFGR & RCC_PLLCFGR_PLLM);
if((RCC->PLLCFGR & RCC_PLLCFGR_PLLSRC) == RCC_PLLCFGR_PLLSRC_HSE)
{
/* Get the I2S source clock value */
i2sclk = (uint32_t)(((HSE_VALUE / pllm) * plln) / pllr);
}
else
{ /* Get the I2S source clock value */
i2sclk = (uint32_t)(((HSI_VALUE / pllm) * plln) / pllr);
}
#endif /* I2S_EXTERNAL_CLOCK_VAL */
/* Compute the Real divider depending on the MCLK output state, with a floating point */
if(I2S_InitStruct->I2S_MCLKOutput == I2S_MCLKOutput_Enable)
{
/* MCLK output is enabled */
tmp = (uint16_t)(((((i2sclk / 256) * 10) / I2S_InitStruct->I2S_AudioFreq)) + 5);
}
else
{
/* MCLK output is disabled */
tmp = (uint16_t)(((((i2sclk / (32 * packetlength)) *10 ) / I2S_InitStruct->I2S_AudioFreq)) + 5);
}
/* Remove the flatting point */
tmp = tmp / 10;
/* Check the parity of the divider */
i2sodd = (uint16_t)(tmp & (uint16_t)0x0001);
/* Compute the i2sdiv prescaler */
i2sdiv = (uint16_t)((tmp - i2sodd) / 2);
/* Get the Mask for the Odd bit (SPI_I2SPR[8]) register */
i2sodd = (uint16_t) (i2sodd << 8);
}
/* Test if the divider is 1 or 0 or greater than 0xFF */
if ((i2sdiv < 2) || (i2sdiv > 0xFF))
{
/* Set the default values */
i2sdiv = 2;
i2sodd = 0;
}
/* Write to SPIx I2SPR register the computed value */
SPIx->I2SPR = (uint16_t)((uint16_t)i2sdiv | (uint16_t)(i2sodd | (uint16_t)I2S_InitStruct->I2S_MCLKOutput));
/* Configure the I2S with the SPI_InitStruct values */
tmpreg |= (uint16_t)((uint16_t)SPI_I2SCFGR_I2SMOD | (uint16_t)(I2S_InitStruct->I2S_Mode | \
(uint16_t)(I2S_InitStruct->I2S_Standard | (uint16_t)(I2S_InitStruct->I2S_DataFormat | \
(uint16_t)I2S_InitStruct->I2S_CPOL))));
#if defined(SPI_I2SCFGR_ASTRTEN)
if((I2S_InitStruct->I2S_Standard == I2S_Standard_PCMShort) || (I2S_InitStruct->I2S_Standard == I2S_Standard_PCMLong))
{
/* Write to SPIx I2SCFGR */
SPIx->I2SCFGR = tmpreg | SPI_I2SCFGR_ASTRTEN;
}
#else
/* Write to SPIx I2SCFGR */
SPIx->I2SCFGR = tmpreg ;
#endif
}
in older version,the same function is
void I2S_Init(SPI_TypeDef* SPIx, I2S_InitTypeDef* I2S_InitStruct)
{
uint16_t tmpreg = 0, i2sdiv = 2, i2sodd = 0, packetlength = 1;
uint32_t tmp = 0, i2sclk = 0;
#ifndef I2S_EXTERNAL_CLOCK_VAL
uint32_t pllm = 0, plln = 0, pllr = 0;
#endif /* I2S_EXTERNAL_CLOCK_VAL */
/* Check the I2S parameters */
assert_param(IS_SPI_23_PERIPH(SPIx));
assert_param(IS_I2S_MODE(I2S_InitStruct->I2S_Mode));
assert_param(IS_I2S_STANDARD(I2S_InitStruct->I2S_Standard));
assert_param(IS_I2S_DATA_FORMAT(I2S_InitStruct->I2S_DataFormat));
assert_param(IS_I2S_MCLK_OUTPUT(I2S_InitStruct->I2S_MCLKOutput));
assert_param(IS_I2S_AUDIO_FREQ(I2S_InitStruct->I2S_AudioFreq));
assert_param(IS_I2S_CPOL(I2S_InitStruct->I2S_CPOL));
/*----------------------- SPIx I2SCFGR & I2SPR Configuration -----------------*/
/* Clear I2SMOD, I2SE, I2SCFG, PCMSYNC, I2SSTD, CKPOL, DATLEN and CHLEN bits */
SPIx->I2SCFGR &= I2SCFGR_CLEAR_MASK;
SPIx->I2SPR = 0x0002;
/* Get the I2SCFGR register value */
tmpreg = SPIx->I2SCFGR;
/* If the default value has to be written, reinitialize i2sdiv and i2sodd*/
if(I2S_InitStruct->I2S_AudioFreq == I2S_AudioFreq_Default)
{
i2sodd = (uint16_t)0;
i2sdiv = (uint16_t)2;
}
/* If the requested audio frequency is not the default, compute the prescaler */
else
{
/* Check the frame length (For the Prescaler computing) *******************/
if(I2S_InitStruct->I2S_DataFormat == I2S_DataFormat_16b)
{
/* Packet length is 16 bits */
packetlength = 1;
}
else
{
/* Packet length is 32 bits */
packetlength = 2;
}
/* Get I2S source Clock frequency ****************************************/
/* If an external I2S clock has to be used, this define should be set
in the project configuration or in the stm32f4xx_conf.h file */
#ifdef I2S_EXTERNAL_CLOCK_VAL
/* Set external clock as I2S clock source */
if ((RCC->CFGR & RCC_CFGR_I2SSRC) == 0)
{
RCC->CFGR |= (uint32_t)RCC_CFGR_I2SSRC;
}
/* Set the I2S clock to the external clock value */
i2sclk = I2S_EXTERNAL_CLOCK_VAL;
#else /* There is no define for External I2S clock source */
/* Set PLLI2S as I2S clock source */
if ((RCC->CFGR & RCC_CFGR_I2SSRC) != 0)
{
RCC->CFGR &= ~(uint32_t)RCC_CFGR_I2SSRC;
}
/* Get the PLLI2SN value */
plln = (uint32_t)(((RCC->PLLI2SCFGR & RCC_PLLI2SCFGR_PLLI2SN) >> 6) & \
(RCC_PLLI2SCFGR_PLLI2SN >> 6));
/* Get the PLLI2SR value */
pllr = (uint32_t)(((RCC->PLLI2SCFGR & RCC_PLLI2SCFGR_PLLI2SR) >> 28) & \
(RCC_PLLI2SCFGR_PLLI2SR >> 28));
/* Get the PLLM value */
pllm = (uint32_t)(RCC->PLLCFGR & RCC_PLLCFGR_PLLM);
if((RCC->PLLCFGR & RCC_PLLCFGR_PLLSRC) == RCC_PLLCFGR_PLLSRC_HSE)
{
/* Get the I2S source clock value */
i2sclk = (uint32_t)(((HSE_VALUE / pllm) * plln) / pllr);
}
else
{ /* Get the I2S source clock value */
i2sclk = (uint32_t)(((HSI_VALUE / pllm) * plln) / pllr);
}
#endif /* I2S_EXTERNAL_CLOCK_VAL */
/* Compute the Real divider depending on the MCLK output state, with a floating point */
if(I2S_InitStruct->I2S_MCLKOutput == I2S_MCLKOutput_Enable)
{
/* MCLK output is enabled */
tmp = (uint16_t)(((((i2sclk / 256) * 10) / I2S_InitStruct->I2S_AudioFreq)) + 5);
}
else
{
/* MCLK output is disabled */
tmp = (uint16_t)(((((i2sclk / (32 * packetlength)) *10 ) / I2S_InitStruct->I2S_AudioFreq)) + 5);
}
/* Remove the flatting point */
tmp = tmp / 10;
/* Check the parity of the divider */
i2sodd = (uint16_t)(tmp & (uint16_t)0x0001);
/* Compute the i2sdiv prescaler */
i2sdiv = (uint16_t)((tmp - i2sodd) / 2);
/* Get the Mask for the Odd bit (SPI_I2SPR[8]) register */
i2sodd = (uint16_t) (i2sodd << 8);
}
/* Test if the divider is 1 or 0 or greater than 0xFF */
if ((i2sdiv < 2) || (i2sdiv > 0xFF))
{
/* Set the default values */
i2sdiv = 2;
i2sodd = 0;
}
/* Write to SPIx I2SPR register the computed value */
SPIx->I2SPR = (uint16_t)((uint16_t)i2sdiv | (uint16_t)(i2sodd | (uint16_t)I2S_InitStruct->I2S_MCLKOutput));
/* Configure the I2S with the SPI_InitStruct values */
tmpreg |= (uint16_t)((uint16_t)SPI_I2SCFGR_I2SMOD | (uint16_t)(I2S_InitStruct->I2S_Mode | \
(uint16_t)(I2S_InitStruct->I2S_Standard | (uint16_t)(I2S_InitStruct->I2S_DataFormat | \
(uint16_t)I2S_InitStruct->I2S_CPOL))));
/* Write to SPIx I2SCFGR */
SPIx->I2SCFGR = tmpreg;
}
differ as picture above, I think there is a problem. Can you help me with it?
2024-07-12 05:55 AM
Hello @Ethan1 ,
The change in packet length calculation seems to be an attempt to correct the prescaler computation for different I2S standards and data formats. The older version might have had issues with certain configurations, leading to incorrect clock settings
Regards