2014-06-24 12:59 AM
I am a little bit confused about the differences between the ''standard peripherals lib'' and the ''stm32cube''.
Here is what I figured out so far: Most of the tutorials I found for the stm32f4xx are using the standard peripherals lib (stm32f4xx_gpio.h
,stm32f4xx_exti.h
), which are the ''old'' libraries. The ''stm32Cube'' seems to be a update ''new'' library version with different include files (stm32f4xx_hal_...) and different functions.
Is my understanding correct ? I cannot run the examples for the ''old'' library when using ''stm32Cube'' installed - is that also correct ? If I am correct with the upper 2 assumptions, where can I get support for the stm32cube-examples ? Please help me in understanding the library issue (...says the beginner...).2014-06-24 3:14 AM
The ''stm32Cube'' seems to be a update ''new'' library version with different include files (
stm32f4xx_hal_...) and different functions.
Is my understanding correct ? The STM32Cube is a new approach for STM32 libraries offering HAL functions which are hardware independent. So you may use the same prototype for almost all products. The STM32Cube comes with the
http://www.st.com/web/en/catalog/tools/PF259242
tool which is a code generator. Please refer tohttp://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00104712.pdf
for more details on how to use it. I cannot run the examples for the ''old'' library when using ''stm32Cube'' installed - is that also correct ? No, you still be able to run examples from both standard library & cube. You need just to have the standard library downloaded locally. If I am correct with the upper 2 assumptions, where can I get support for the stm32cube-examples ?For any help regarding STM32Cube or Standard library, please submit your request on the forum ''[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx]STM32 Software Tools and Firmware''. Best Regards -Mayla-
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.