Control TIMER interrupts- STM32F4 discovery board
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-06-24 3:06 AM
Posted on June 24, 2014 at 12:06
This is my program to control TIMER2 interrupt but it doesn't jump into interrupt function. How can I fix this problems?????
I used startup_stm32f4xx.s , set clock for timer2, enable timer2 interrupt in NVIC register./************************************************************/void TIM2_IRQHandler(void){ if(timer2->TIMx_SR & 0x1){ gpio_toggle_off(gpio_A,GPIO_Pin_1); number_display(gpio_D,number0); } timer2->TIMx_SR=0x0;}__declspec(noreturn) void main(void) {gpio_setlock(rcc,GPIOD_CLOCK); /*PORT-A enable*/
gpio_setlock(rcc,GPIOA_CLOCK); /*PORT-B enable*/ timer_setlock(rcc,TIMER_2); /* TIMER2 enable*/ //timer_interrupt(timer2,interrupts); NVIC->ISER[0]|= 1<<(TIM2_IRQn); // enable timer_interrupt =28 timer2->TIMx_PSC =41999; // prescaler timer2->TIMx_DIER |=0x01; // enable update interrupt timer2->TIMx_ARR =1999; // counting number timer2->TIMx_CR1 |=0x90; // auto reload, count down timer2->TIMx_CR1 |=0x01; // enable counter timer2->TIMx_EGR =0x01; // update generation while(1);}/***************************************************************/ #stm32f4 #discovery
Labels:
- Labels:
-
STM32F4 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0