2018-04-30 4:32 AM
Hi guys,
I'm using the
STM32L475RCT
in a custom board. When using the JLink everything is working fine but when I discounnect the Jlink and power cycle the board the application doesn't work at all. Each time I have to force NRST to 0 and release it in ordre to make the application works.I have 100nF capacitor between the NRST pin and GND as recommended in ST datasheet(
6.3.15
).I checked the voltage on the NRST pin and it seems correct : it goes from 0.358V to 3.1V in ~4ms at board power up which follow the required low level voltage ( VIL(NRST) =0.3?VDDIOx = 0.984V) and high level reset voltage ( VIH(NRST) = 0.7?VDDIOx = 2.29V).
Any thoughts on where the problem might be ?
#stpm32-reset #reset #stm32l4 #nrst #reset-problemSolved! Go to Solution.
2018-05-02 4:06 AM
Guys, I figured out.
I connected the BOOT0 to GND and the standalone application started working without the JLINK.
Not sure the reason of this since in the manual leaving BOOT0 NC won't have an effect on the startup sequence ! I think I'll need to do more reading on this subject.
Thank you for the help
2018-04-30 5:31 AM
I would look at what you are doing with the supply pins, especially VDDA, and if you have multiple supplies. Check initial rise times on a scope with respect to NRST.
Consider using a POR chip like the MCP120 to threshold on the slowest supply.
2018-04-30 8:20 AM
Thank you for your response,
I have a single 3.3V powering all the VDD and VDDA pins with 100nF capacitor for each pin.
I forget to mention that I checked both the V3.3 and NRST rise time and they were fine. here is a screenshot
I have the same circuit working with no issues on the STM32F417 !
2018-04-30 8:41 AM
Double-check if all the ground (including analog) and supply pins are connected - this includes checking for bad solder joints.
JW
2018-04-30 8:42 AM
>>I have the same circuit working with no issues on the STM32F417 !
Well not work here, so you'll need to change something.
I would suggest a 10K pull-up on the NRST pin, and a 10K pull-down on BOOT0
2018-04-30 10:20 AM
Thx, I did and circuit seems okey. I have the same issue with the 4 prototype boards !
2018-04-30 10:27 AM
I have tried 10K pull up on the NRST and connecting the BOOT0 to GND (I do that on other boards) and still getting the same behavior!
Wonder If a delay between the rising of the V3.3 and NRST is necessary ? I doubled checked the curves and got the below figure :
Blue : NRST
red : 3.3V
When I force the NRST to 0 and turn on the power supply and just after I release manually the NRST pin, the application run right away!
2018-04-30 11:39 AM
Are you sure it is not running, and just stuck somewhere early in your code?
I would try perhaps adding a delay in Reset_Handler, driving a GPIO, or jumping to the System Loader ROM, and seeing if I could get the USART to respond or USB/DFU coming up. Sorry, got very little insight into your design.
2018-05-01 5:53 PM
I use a reset chip.
2.93V before 1.2Second timer then it releases Reset.
never have a problem with Reset again.
2018-05-02 3:50 AM
Clive One wrote:
Are you sure it is not running, and just stuck somewhere early in your code?
I would try perhaps adding a delay in Reset_Handler, driving a GPIO, or jumping to the System Loader ROM, and seeing if I could get the USART to respond or USB/DFU coming up. Sorry, got very little insight into your design.
I tried to turn on an LED first thing in main() but it didn't work.
I introduced a delay aswell (in main) but still not working.
Are you interested in checking the design ?