ST32L476 use of VREF+
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-02-02 8:01 AM
Thanks for any help. I'm confused on how to connect VREF+. I see that it can be used as an reference voltage output, and I now have it as No Connect. VDDA is connected to its pin, which seems to provide the voltage reference needed for the ADC.
So, my question: Is this enough for the ADC to work (VREF+ No Connect)? We're about to roll with boards, and I'd rather not do an ECO at this point, but I'd also rather have it work :)- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-02-02 8:29 AM
Even if you intend to use the internal voltage reference, the datasheet requires you to connect a typ.1uF capacitor (see ''VREFBUF characteristics'').
You should've read also AN4555. JW- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-02-02 9:39 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-02-02 1:40 PM
> And if I want to use VDDA as the reference voltage (and not use the internal), do you think I can just tie VREF+ to VDDA?
Of course you can - it's what ST does on smaller packages, anyway, inside the package. > What would the consequences be -- some potential noise on VREF? Noise and fluctuations (which at the end of the day is the same, at different frequencies). Absolute precision can be checked/compensated using the internal reference. VDDA does not source heavy logic - that's what VDD is for - so it may be almost as good as a separate external reference, if VDDA is properly designed for. Don't forget about quite grounds, too, especially VSSA. Have you consulted that appnote? Also be prepared for quite a significant noise in the ADC itself. Read thoroughly the values given in the datasheet, these add up to the proportion of VREF noise. > Pardon my ignorance, this is my first foray into digital. But, isn't ADC as analog as it gets, in the realm of microcontrollers? ;) Jan- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-02-05 1:15 PM
Funny!
Thanks for the help Jan.