cancel
Showing results for 
Search instead for 
Did you mean: 

ST Nucleo F767ZI USB not detected by PC

out
Associate

I've compiled my first program and I can't find a way to upload to the board.
When I plug the USB, the onboard LED is lit, but my PC does not detect anything - I don't hear any "plug" sound, and I can't find any device in Device Manager (recognized nor not recognized).

I've tried different cables, different USB ports, and a different PC. 
Is the board damaged?
The default program is fine, I can use user button to switch LEDs.

This is my first STM32 :(

out_0-1719742246496.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Chief II

:)

You have to connect the PC (with a working data cable) just to the st-link (what you name 5VDC in your pic.).

Then try...

 

ps. Reading the manual could also help... :)

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
AScha.3
Chief II

:)

You have to connect the PC (with a working data cable) just to the st-link (what you name 5VDC in your pic.).

Then try...

 

ps. Reading the manual could also help... :)

If you feel a post has answered your question, please click "Accept as Solution".

Thanks, that worked, but I also had to change the cable.
I was following a text next to USB sockets, that is USB PWR and USB USER.
Never thought USB PWR is meant to be programming interface xd