2024-10-27 7:35 PM
Hello.
Is there an example F/W for STEVAL-ESC001V1 or X-NUCLEO-IHM08M1 that is SPL compatible?
I need to continue to use the Standard Peripheral Library (SPL) to utilize the existing code.
If there is a way to create or convert the project by X-CUBE-MCSDK to SPL compatible, that would be the best.
Thank you!