2014-02-10 1:39 AM
Hi
I'm using STM32F373x SPI in slave mode. I get errors in about 0.1% bits transmitted, occurs in 50% of units from first production series of custom board. SPI lines have RC filter installed to improve EMC immunity. Rise/fall times are about 1us with filters and 10ns without them. I get no errors without filters. My question is what parameter do I exceeded?Table 58 defines max. rise/fall 8ns (I guess only for master, cause load is also described). I think I'm not getting out of 30-70% duty cycle. Speed is 190kHz, reducing to 80kHz didn't changed anything. #eye-pattern #stm32-spi2014-02-13 5:24 AM
waclawek.jan:
Many thanks for detailed information.I knew that SPI is not intended for longer distances and we could live with this cheap and fast medium for our purposes. I never thought about it, I guess SPI hardware has some more hysteresis. I'll keep it in mind for future projects.Today I can't recreate this errors (using exactly the same hardware and power supplies as for last week). I'll write when we decide which solution is sufficient for our needs.2014-02-13 5:39 AM
BTW I used similar SPI with board to board connection in older projects without problems (different uC). Now I checked details and it looks like Atmel AVR has much different (better for my purposes) Slave hardware, including clock sampling and max. Slave slope allowed 1.6us.