2026-01-21 9:34 PM - last edited on 2026-01-22 1:15 AM by Andrew Neil
Hi, in this STM32L4Q5RGT6 microcontroller of (LQFP48) package how many SPI, QSPI should be connected.
Solved! Go to Solution.
2026-01-22 12:13 AM
Hello @abhishek_25;
Your are welcome. Thank you for your contribution in STCommunity.
Please click on Accept as Solution on the reply which solved your issue or answered your question.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-21 11:33 PM
Hello @abhishek_25 and welcome to the community;
According STM32L4Q5 datasheet; STM32L4Q5RGT6 supports 3 SPIs and maximum 2 OCTOSPIs (available only on multiplexed mode).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-21 11:37 PM
Hi Kaouthar
so can I use two spi and 1 qspi in LQFP48 package.
2026-01-21 11:40 PM
Hello,
Yes, you can.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-21 11:49 PM
Appreciate your prompt responses.
Thank you
2026-01-22 12:13 AM
Hello @abhishek_25;
Your are welcome. Thank you for your contribution in STCommunity.
Please click on Accept as Solution on the reply which solved your issue or answered your question.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.