2014-03-01 9:26 AM
The registers aren't getting affected when I run the following code on the board. The clock is getting set however the SPI->CR1 register is not getting affected at all, upon debugging the code it shows only 0's.
&sharpinclude <stm32f2xx.h>
&sharpinclude <GPIO_STM32F2xx.h>//&sharpinclude ''SPI_STM32F2xx.c''void init123(){ RCC->AHB1ENR |= (0x01); //IO port A clock enable for GPIO Pins for MOSI,MISO and SCK GPIO_PinConfigure(GPIOA,5,GPIO_MODE_AF,GPIO_OUTPUT_PUSH_PULL,GPIO_OUTPUT_SPEED_50MHz,GPIO_NO_PULL_UP_DOWN); //For PA5 GPIO_PinConfigure(GPIOA,6,GPIO_MODE_AF,GPIO_OUTPUT_PUSH_PULL,GPIO_OUTPUT_SPEED_50MHz,GPIO_NO_PULL_UP_DOWN); //For PA6 GPIO_PinConfigure(GPIOA,7,GPIO_MODE_AF,GPIO_OUTPUT_PUSH_PULL,GPIO_OUTPUT_SPEED_50MHz,GPIO_NO_PULL_UP_DOWN); //For PA7 //For configuring the above pins in SPI GPIO_PinAF (GPIOA,5,GPIO_AF_SPI1); GPIO_PinAF (GPIOA,6,GPIO_AF_SPI1); GPIO_PinAF (GPIOA,7,GPIO_AF_SPI1); RCC->AHB1ENR |= (0x01<<3); //IO port E clock enable fr GPIO Pins for Chip Select GPIO_PinConfigure(GPIOE,7,GPIO_MODE_OUTPUT,GPIO_OUTPUT_PUSH_PULL,GPIO_OUTPUT_SPEED_50MHz,GPIO_PULL_UP); //For Chip Select - PE7 GPIOE->BSRRL |= (0x01<<6); //For setting PE7 High SPI1->CR1 &= ~(0x01<<6); //SPI Enable RCC->APB2ENR |= (0x01<<11); //SPI clock enable SPI1->CR1 &= ~(0x01<<15); //Full Duplex mode SPI1->CR1 |= (0x01<<2); //SPI in Master Mode SPI1->CR1 &= ~(0x01<<11); //8 bit data format SPI1->CR1 &= ~ (0x01<<1); // CPOL - 0 SPI1->CR1 |= 0x01; // CPHA - 1 SPI1->CR1 &= ~(0x111<<3); //Baud Rate 000 config SPI1->CR1 &= ~ (0x01<<6); // MSB First SPI1->CR1 |= (0x01<<6); //SPI Enable }uint8_t send123(uint8_t data){ SPI1->DR=data; while (!(SPI1->SR & 0x10)); // wait until transmit complete while (!(SPI1->SR & 0x01)); // wait until receive complete while (!(SPI1->SR & 0x01<<6)); // wait until SPI is not busy anymore return SPI1->DR;}int main(void){ uint8_t received_val = 0; init123(); while(1) { GPIOE->BSRRL |= (0x01<<6); //For setting PE7 Low send123(0xAA); // transmit data received_val = send123(0x00); // transmit dummy byte and receive data GPIOE->BSRRL |= (0x01<<6); //For setting PE7 High }} #spi #stm32f2xx #stm32f2xx #spi2014-03-01 1:34 PM
RCC->APB2ENR |= (0x01<<11); //SPI clock enable
Isn't 0x1000 (1 << 12) ?, plus you really should do it several instructions prior to programming the peripheral.2014-03-01 11:21 PM
Thank you so much, that worked! I moved the SPI clock enable right after the configuration of the GPIO pins for SPI.
I am working on SPI for the first time and also I have no prior experience with this board.I am trying to test the SPI code by sending and receiving data to/from MSP430F54388. When I run the code I am unable to send the data. The MODF bit in the status register gets set. The code gets stuck on the while loop (at the part where it is waiting for the transmit buffer to become empty)Any suggestions?I just want to test SPI, can you suggest another way to do it? Like a loopback or something? And if at all there is a way to do loopback then how do I proceed? By connecting the MISO and MOSI together? What about the Clock and the Chip Select?