2021-03-06 04:10 AM
Hi everyone,
I am working with the SPI in slave mode on an STM32G071 and having some trouble with the different SPI modes. I set both CPOL and CPHA to 0 during initialization:
SPI_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX;
SPI_InitStruct.Mode = LL_SPI_MODE_SLAVE;
SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_8BIT;
SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_LOW;
SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE;
SPI_InitStruct.NSS = LL_SPI_NSS_HARD_INPUT;
SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST;
SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
SPI_InitStruct.CRCPoly = 7;
LL_SPI_Init(SPI1, &SPI_InitStruct);
According to the datasheet (see attached image) I would expect the data to be loaded on falling edge and sampled on rising edge. When I send a 0x81, I get the signal from the second attached image. Obviously the data is updated during rising edge and sampled on the falling edge. What am I missing here?
2021-03-08 11:26 PM
Read out and check/post the SPI registers content.
JW
2021-03-09 12:29 AM
Here are the registers after initialization. Looks fine to me.
Edit: Ohh sorry, that was just the initialization, before enabling it. This will also set the SPE bit in CR1, everything else stays the same.
2021-03-09 03:34 AM
Try to observe the signals on oscilloscope.
Try a different (lower) baudrate.
Try to increase drive (OSPEEDR), first at slave's MISO, then master's SCK (but carefully, if the master is a high speed IO, highest speeds may be detrimental if you don't have proper termination).
You don't connect master and slave with flying leads, do you? If so, make sure it's as short as possible, and there's a return (ground) to each signal separately (best twisted with its signal).
JW