cancel
Showing results for 
Search instead for 
Did you mean: 

SPI function of STM32F746 to perform half-duplex communication-3

勝後藤.1
Associate II

hello,

Should I use TXFIFO or RXFIFO to send and receive SPI data in a continuous flow?

In that case, do I have to enable CRC calculation?

If you have to enable CRC calculation

I don't want to send or receive CRC data.

Is there any other way?

Goto​

0 REPLIES 0