cancel
Showing results for 
Search instead for 
Did you mean: 

SPI - DMA - NUCLEOH743ZI

Antal Soos
Associate
Posted on May 16, 2018 at 20:06

In NUCLEO-H743ZI  environment using the STM32CubeMX the:

HAL_SPI_Receive_DMA(&hspi1, (uint8_t*)u8SpiRxBuffer, SIZE) 

function in Master Mode.

It generates the clocks on the output pin correctly up to 16 byte of data.

If the SIZE is more than 16 it got disregarded, even if the data size in SPI get changed to word format and SIZE set to 5 the total clock generated is 16*8  =128.

Any suggestion?

Thanks

Antal

#dma #nucleo-h743zi #spi
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0