2018-05-10 12:28 AM
STM32L452C
My code:
__HAL_RCC_CRC_CLK_ENABLE();
CRC->POL = (uint32_t) 0x1021;//CRC-16-CCITT CRC->INIT = (uint32_t) 0xFFFF; CRC->CR = (uint32_t) 0x09;//REV_OUT = 0, REV_IN = 00, POLYSIZE = 01, RESET = 1 CRC->DR = '1'; CRC->DR = '2'; CRC->DR = '3'; CRC->DR = '4';The correct result for this CRC is 0x5349 but when I read the DR I get 0xb23b
I have tried all combinations of input and output bit reversal, doesn't work.
2018-05-10 1:18 AM
Hi
robert.015
,I recommend you to have a look to CRC examples under the STM32L4 firmware package, it may helpful to start your own project:STM32Cube_FW_L4_V1.0\Projects\NUCLEO-L452RE\Examples\CRC
-Nesrine-
2018-05-10 3:59 AM
Thanks. I just realised that the cubeMX utility doesn't copy all the HAL drivers to your project dir. I was missing 'stm32l4xx_hal_crc.c' etc.
2018-05-16 8:55 AM
DR is a 32-bit wide register, you need to write bytes 8-bit wide, thusly...
*((volatile uint8_t *)&CRC->DR) = '1';
2018-05-16 10:48 AM
Could you please precise the MX version are you using?
if your are using an older version please use the latest one and tell us if the issue still again