cancel
Showing results for 
Search instead for 
Did you mean: 

Is the STM32H7 intended to replace F7 family?

John F.
Senior
Posted on January 31, 2018 at 16:50

Is the STM32H7 intended to replace F7 family? I want to start a design and considered the F7 family but will it disappear when the H7 is in full production?

#stm32h7 #stm32f7
This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Posted on January 31, 2018 at 17:05

I doubt it, the variety of parts allows for price stratification, and attack different markets.

The 400 MHz speed makes it competitive against the ATMEL/MICROCHIP CM7 parts which have been 300 MHz FPU-D since inception.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on January 31, 2018 at 17:07

Also publically committed to the STM32F7 thru January 2027

http://www.st.com/content/st_com/en/support/resources/product-longevity.html

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Khouloud GARSI
ST Employee
Posted on January 31, 2018 at 17:24

Hello

FitzGerald.John

,

The STM32F7 and STM32H7 are two distinct families. They will coexist on the market.

You can pursue your design based on our STM32F7 device without concerns.

Khouloud.

John F.
Senior
Posted on February 01, 2018 at 09:06

Thanks Clive and Khouloud for the quick replies and helpful information.

Posted on February 01, 2018 at 10:44

Hi Khoulound,

We know that the ST will not stop producing STM32F7 that have already been released. The question is: Will all future cortex-m7 releases be in the STM32H7 family? Or will there be new releases in the STM32F7 family as well?

Ari.

Posted on February 01, 2018 at 11:14

Hello

Mendes.Ari

‌,

We are providingdifferent STM32F7 lines offering various features.

Shall I understand that you have a particular use case that can not be realized using the STM32F7 MCUs already existing on the market?

Khouloud.

T J
Lead
Posted on February 01, 2018 at 12:33

as far as I can see, the H7 will drop in on an existing F7 PCB.

I checked the 208pin LQFP, and every pin looks good. FMC pins, Ethernet MII, USB Device/Host, Spi,IIC,Uarts,DSI all line up, pin for pin.

Posted on February 01, 2018 at 12:57

Yes,

 I hope for a STM32 for high-end  Motor control and digital power convertion. Something like the STM32F303/334 but using a cortex-m7 core and with ethernet peripheral. STM32H7 do the job, but it is very expensive and complex for that. 

 Ari.

Frederic LE CAM
ST Employee
Posted on February 08, 2018 at 03:31

The STM32F7 family is a large portfolio covered by the 10 years longevity comittment as advertized by ST for the whole STM32 family so there is absolutely  no issue to start a new design with any member of this series. The many STM32 series are based upon different technology nodes depending on the objectives that are targeted for the given series, be it the performance, be it  the low power consumption or any other combination. On the high performance path, the STM32H7 platform will see some other variants proposed in the future to expand the offering.