2015-07-06 9:18 AM
I am trying to use the SPI interface with a SPI temperature sensor and the STM32L Discovery board. I want to make a very basic read operation. I have set SPI_CLK to PA5 , MISO to PA11 and MOSI to PA12. The CS is controlled with the Digital Output Pin PA4.
However, after configuration, when I call the read procedure nothing works and only the CS pin works correctly (the other MISO MOSI CLK pin remain low).Following are the procedures used to initialize SPI and call a read operation:void SPI_initialization(void){ RCC_APB2PeriphClockLPModeCmd(RCC_APB2Periph_SPI1, ENABLE); SPI_InitTypeDef SPI_InitTypeDefStruct; SPI_InitTypeDefStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitTypeDefStruct.SPI_Mode = SPI_Mode_Master; SPI_InitTypeDefStruct.SPI_DataSize = SPI_DataSize_8b; SPI_InitTypeDefStruct.SPI_CPOL = SPI_CPOL_High; SPI_InitTypeDefStruct.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitTypeDefStruct.SPI_NSS = SPI_NSS_Soft; SPI_InitTypeDefStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64; SPI_InitTypeDefStruct.SPI_FirstBit = SPI_FirstBit_MSB; SPI_Init(SPI1, &SPI_InitTypeDefStruct); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); GPIO_InitTypeDef gpioStructure; gpioStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_11 | GPIO_Pin_12; gpioStructure.GPIO_Mode = GPIO_Mode_AF; gpioStructure.GPIO_OType = GPIO_OType_PP; gpioStructure.GPIO_Speed = GPIO_Speed_40MHz; GPIO_Init(GPIOA, &gpioStructure); gpioStructure.GPIO_Pin = GPIO_Pin_4; gpioStructure.GPIO_Mode = GPIO_Mode_OUT; gpioStructure.GPIO_OType = GPIO_OType_PP; gpioStructure.GPIO_PuPd = GPIO_PuPd_UP; gpioStructure.GPIO_Speed = GPIO_Speed_40MHz; GPIO_Init(GPIOA, &gpioStructure); GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource11, GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource12, GPIO_AF_SPI1); GPIO_SetBits(GPIOA, GPIO_Pin_4); SPI_Cmd(SPI1, ENABLE);}uint16_t mySPI_GetTemp(void){uint8_t high8b_temp, low8b_temp;uint16_t my16b_temp;GPIO_ResetBits(GPIOA, GPIO_Pin_4);uint8_t adress = 0b01010000;while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);SPI_I2S_SendData(SPI1, adress);while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE));SPI_I2S_ReceiveData(SPI1); //Clear RXNE bitwhile(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);SPI_I2S_SendData(SPI1, 0x00); //Dummy byte to generate clockwhile(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE));high8b_temp = SPI_I2S_ReceiveData(SPI1);while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);SPI_I2S_SendData(SPI1, 0x00); //Dummy byte to generate clockwhile(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE));low8b_temp = SPI_I2S_ReceiveData(SPI1);GPIO_SetBits(GPIOA, GPIO_Pin_4);my16b_temp = (uint16_t)(high8b_temp<<8);my16b_temp = my16b_temp | low8b_temp;return my16b_temp;}Anyone can help?Thanks.2015-07-06 10:01 AM
It looks like you have only enabled the Low Power Mode clock in the RCC domain.
RCC_APB2PeriphClockLPModeCmd(RCC_APB2Periph_SPI1, ENABLE);
add or change this too:RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);
-Kirem