[Solved] Linker script: block RAM for variables
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-04 11:09 AM
How do I have to configure the linker script file to block the required space
for Ethernet buffers at 0x24000000?
STM32H743 starts with DTCM at 0x20000000, but Ethernet works in 0x24000000 only.
I want to use the RAM space around for my purpose without losing so much.
In ethernetif.c the buffers are marked with .RxDecripSection, .TxDecripSection, .RxArraySection.
I'm not a linker file specialist to make the right definitions.
Thank you for your help.
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-07 2:44 PM
Solved with HAL 1.2.0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-06 2:16 AM
I modified the linker script file for myself to place ETH descriptors and RX buffer in one SRAM block. It's so much fun so I did it for the UART buffer as well in another SRAM section for DMA transfer.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-06 4:22 AM
Posted on October 06, 2017 at 11:22
Hi
Wagner.Joerg
,
https://community.st.com/0D50X00009bMM5DSAW
-Nesrine-
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-06 4:33 AM
to help us lesser able programmers;
how did you do it ?
that chip is not available at Digikey..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-06 4:55 AM
I have a NUCLEO-H743ZI board. IDE is OpenSTM32 (GNU C). For Keil and IAR there is nothing to do.
My linker script file looks like:
/* Entry Point */
ENTRY(Reset_Handler)/* Highest address of the user mode stack */
_estack = 0x20020000; /* end of RAM *//* Generate a link error if heap and stack don't fit into RAM */_Min_Heap_Size = 0x200; /* required amount of heap */_Min_Stack_Size = 0x400; /* required amount of stack *//* Specify the memory areas */
MEMORY{DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128KRAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512KRAM1_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 128KRAM2_D2 (xrw) : ORIGIN = 0x30020000, LENGTH = 128KRAM3_D2 (xrw) : ORIGIN = 0x30040000, LENGTH = 32KRAM4_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64KITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64KFLASH (rx) : ORIGIN = 0x8000000, LENGTH = 2048K}/* Define output sections */
SECTIONS{ /* The startup code goes first into FLASH */ .isr_vector : { . = ALIGN(4); KEEP(*(.isr_vector)) /* Startup code */ . = ALIGN(4); } >FLASH/* The program code and other data goes into FLASH */
.text : { . = ALIGN(4); *(.text) /* .text sections (code) */ *(.text*) /* .text* sections (code) */ *(.glue_7) /* glue arm to thumb code */ *(.glue_7t) /* glue thumb to arm code */ *(.eh_frame)KEEP (*(.init))
KEEP (*(.fini)). = ALIGN(4);
_etext = .; /* define a global symbols at end of code */ } >FLASH/* Constant data goes into FLASH */
.rodata : { . = ALIGN(4); *(.rodata) /* .rodata sections (constants, strings, etc.) */ *(.rodata*) /* .rodata* sections (constants, strings, etc.) */ . = ALIGN(4); } >FLASH.ARM.extab : { *(.ARM.extab* .gnu.linkonce.armextab.*) } >FLASH
.ARM : { __exidx_start = .; *(.ARM.exidx*) __exidx_end = .; } >FLASH.preinit_array :
{ PROVIDE_HIDDEN (__preinit_array_start = .); KEEP (*(.preinit_array*)) PROVIDE_HIDDEN (__preinit_array_end = .); } >FLASH .init_array : { PROVIDE_HIDDEN (__init_array_start = .); KEEP (*(SORT(.init_array.*))) KEEP (*(.init_array*)) PROVIDE_HIDDEN (__init_array_end = .); } >FLASH .fini_array : { PROVIDE_HIDDEN (__fini_array_start = .); KEEP (*(SORT(.fini_array.*))) KEEP (*(.fini_array*)) PROVIDE_HIDDEN (__fini_array_end = .); } >FLASH/* used by the startup to initialize data */
_sidata = LOADADDR(.data);/* Initialized data sections goes into RAM, load LMA copy after code */
.data : { . = ALIGN(4); _sdata = .; /* create a global symbol at data start */ *(.data) /* .data sections */ *(.data*) /* .data* sections */. = ALIGN(4);
_edata = .; /* define a global symbol at data end */ } >DTCMRAM AT> FLASH/* Uninitialized data section */ . = ALIGN(4); .bss : { /* This is used by the startup in order to initialize the .bss secion */ _sbss = .; /* define a global symbol at bss start */ __bss_start__ = _sbss; *(.bss) *(.bss*) *(COMMON)
. = ALIGN(4);
_ebss = .; /* define a global symbol at bss end */ __bss_end__ = _ebss; } >DTCMRAM/* User_heap_stack section, used to check that there is enough RAM left */
._user_heap_stack : { . = ALIGN(8); PROVIDE ( end = . ); PROVIDE ( _end = . ); . = . + _Min_Heap_Size; . = . + _Min_Stack_Size; . = ALIGN(8); } >DTCMRAM.RxDecripSection (NOLOAD) :
{ . = 0x00; *(.RxDecripSection) *(.RxDecripSection*) } >RAM2_D2 .TxDecripSection (NOLOAD) : { . = 0x60; *(.TxDecripSection) *(.TxDecripSection*) } >RAM2_D2 .ETHfill (NOLOAD) : { . = 0xe0; } >RAM2_D2 .RxArraySection (NOLOAD) : { . = 0x200; *(.RxArraySection) *(.RxArraySection*) } >RAM2_D2 .DMA_UART3STR (NOLOAD) : { . = 0x2000; *(.DMA_UART3STR) *(.DMA_UART3STR*) } >RAM3_D2/* Remove information from the standard libraries */
/DISCARD/ : { libc.a ( * ) libm.a ( * ) libgcc.a ( * ) }.ARM.attributes 0 : { *(.ARM.attributes) }
}I used Dx for the domain numbers.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-07 2:44 PM
Solved with HAL 1.2.0