2024-01-01 11:00 PM - last edited on 2024-01-01 11:10 PM by mƎALLEm
主控板 (SMT32F407VGT6)与同服板 (STM32F407VGT6) 之间的CAN通讯,环境温度低于-10度,通讯不正常,环境温度高过-10度!
2024-01-01 11:10 PM
Hello @JACK00 ,
In next time, could you please describe your issue in English as other community members can help you?
Translation:
"The CAN communication between the main control board (SMT32F407VGT6) and the server board (STM32F407VGT6), the ambient temperature is lower than -10 degrees, the communication is abnormal, and the ambient temperature is higher than -10 degrees!"
Not sure the question is clear. Could you please elaborate more?
2024-01-01 11:13 PM
The CAN communication between the main control board (SMT32F407VGT6) and the same server board (STM32F407VGT6) shows that the ambient temperature is below -10 degrees, the communication is abnormal, and the ambient temperature is above -10 degrees! Immediately returning to normal, may I ask what the reason is? Confirm that the CAN communication interface hardware chip meets the requirements!
2024-01-01 11:43 PM
Dupe https://community.st.com/t5/stm32-mcus-products/smt32f407vgt6/td-p/624102
2024-01-29 8:36 AM
What is your clock source? HSI or HSE?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.