cancel
Showing results for 
Search instead for 
Did you mean: 

Slave timer configuration procudes an interrupt STM32f10x

JJohn.3
Associate II
int Pulse(void)
 
{
 
TIM_TimeBaseInitTypeDef     TimeStruct; 
 
 
            RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2,ENABLE);
 
    
 
            TIM_SelectInputTrigger(TIM2,TIM_TS_ITR3);//     
 
            TIM_SelectSlaveMode(TIM2,TIM_SlaveMode_External1);
 
 
            TimeStruct.TIM_Prescaler=0;
 
            TimeStruct.TIM_CounterMode=TIM_CounterMode_Up;
 
            TimeStruct.TIM_Period=29;
 
            TimeStruct.TIM_ClockDivision=TIM_CKD_DIV1;
 
            TimeStruct.TIM_RepetitionCounter=0;
 
            TIM_TimeBaseInit(TIM2, &TimeStruct);
 
            TIM_ITConfig(TIM2,TIM_IT_Update,ENABLE);
 
    
 
        ///Master Configuration code
 
...
 
 
 
}
 
 
void TIM2_IRQHandler(){
 
 
   if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET)
 
   {    
 
    x=x+1;   
 
    TIM_ClearITPendingBit(TIM2, TIM_IT_Update);
 
   }
 
    
 
}

I am going to config a master and slave configuration under STM32f10x. I connected them correctly but at the first step it generates an interrupt before enabling the master timer or enable the slave timer. Here is my code:

after calling the Pulse function, it generates TIM2 interrupt(x=1), I need to know why it generates an interrupt when its trigger source is not configured/enabled.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

No, setting PSC or CNT alone won't cause interrupt. It's every time you (and by "you" I here mean also "the library function you are calling") set TIMx_EGR.UG, it sets the Update flag (which can cause interrupt if enabled).

The "library" function does it because setting PSC won't change the prescaler immediately, as PSC is preloaded. Read the TIM chapter in RM.

JW

View solution in original post

3 REPLIES 3
waclawek.jan
Super User

This is consequence of the called library setup function setting TIMx_EGR.UG.

JW

JJohn.3
Associate II

Thank you very much, it works fine, could you let me know about the role of this (EGR) register?does it mean every time that I changed the PSC or counter it makes an interrupt?

waclawek.jan
Super User

No, setting PSC or CNT alone won't cause interrupt. It's every time you (and by "you" I here mean also "the library function you are calling") set TIMx_EGR.UG, it sets the Update flag (which can cause interrupt if enabled).

The "library" function does it because setting PSC won't change the prescaler immediately, as PSC is preloaded. Read the TIM chapter in RM.

JW