cancel
Showing results for 
Search instead for 
Did you mean: 

Shared SDRAM via FMC with dual core stm32h745

SNort.1
Associate II

I am seeing the same issue as this question here :

https://community.st.com/s/question/0D53W00000HyV6FSAV/fmc-with-dual-core-stm32h745

I can configure SDRAM access on the STM32H745 for the M7, but when running two cores I cannot get access from the M4 to work at all.

I note that the thread was never resolved.

Is there any guidance documentation on how to configure this, or any sample projects that show both cores accessing SDRAM?

0 REPLIES 0