cancel
Showing results for 
Search instead for 
Did you mean: 

Setting up a UART caused device reset

Jemegen
Associate III
I am trying to build a uart implementation from scratch to learn the Stm32, but such a code implementation seems to cause my Stm32F030 to go into Reset_Handler state.
What might be wrong with my code? Thanks in advance!

 

 

void uar2_rx_tx_init(void) { USART2->CR1 = (USART_CR1_TE | USART_CR1_UE | USART_CR1_RE | USART_CR1_RXNEIE | USART_CR1_TCIE | USART_CR1_TXEIE); RCC->AHBENR |= RCC_AHBENR_GPIOAEN; RCC-> APB1ENR |= UART2EN; GPIOA->MODER ^= ~(1U<<6); GPIOA->MODER |= (1U<<7); GPIOA->AFR[0] |= (1U<<12); GPIOA->AFR[0] &= ~(1U<<13); GPIOA->AFR[0] &= ~(1U<<14); GPIOA->AFR[0] &= ~(1U<<15); //USART2->CR3 |= RCC_CFGR3_USART2SW_SYSCLK; uart_set_baudrate(USART2, APB_FREQ, UART_BAUDRATE); } uint16_t uart2_read(void) { while(!(USART2->ISR & USART_CR1_RXNEIE)) { } return USART2->RDR; } static void uart_set_baudrate( USART_TypeDef *USARTx, uint32_t PeriphClk, uint32_t BaduRate) { USARTx->BRR = compute_set_baudrate(PeriphClk, BaduRate); //USARTx->BRR = 0x45; } static uint32_t compute_set_baudrate(uint32_t PeriphClk, uint32_t BaudRate) { return ((PeriphClk + (BaudRate/2U)) / BaudRate) ; }​
View more

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

^ means XOR. You probably want &, i.e. AND.

JW

View solution in original post

5 REPLIES 5
waclawek.jan
Super User

> such a code implementation seems to cause my Stm32F030 to go into Reset_Handler state.

At which line?

JW

I tried to attach my debugger and I can tell this code is causing reset:

 

GPIOA->MODER ^= ~(1U<<6);

 

To be exact, it's command at 0x08000368

1.jpg

You'd want to enable the USART2 clock, before writing register.

Check external connectivity to see if that triggers a short or reset.

Doing multiple RMW is also not very efficient. Fold so there's a single load/store instead of multiple.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User

^ means XOR. You probably want &, i.e. AND.

JW

Jemegen
Associate III

It works! Thanks for your help!