2018-12-17 8:30 AM
Hello,
How can I set the STM32L476 LPUART TX to level 1 while the device is in StopMode2?
The LPUART clock is the LSE clock.
Best regards
Mich.
2018-12-26 3:36 AM
Hello Michel,
During the STOP 2 the CPU is clocked-off, you cannot set the LPUART configuration.
To do this, you must wake up from STOP 2, define your configuration and enter it again..
Best regards,
Mohamed Aymen.
2018-12-26 4:06 AM
The cubeMX exemple only uses HSI clock. During the stop mode 2 the LPUART TX pin stays at level 1.
2019-01-04 8:06 AM
Hello Michel,
Which register do you use to set the LPUART TX pin level ?
Best Regards,
Mohamed Aymen.
2019-01-04 8:10 AM
I do not use register to set TX pin level.
I received an help from the distributor. Issue was related to a too fast enter in stop mode.
2019-01-04 8:36 AM
Hi Michel,
Glad to see that you resolved your issue.
It would be helpful for other members to share your experience and provide more details on how you fixed it.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.