2009-03-26 11:54 AM
Self written bootloader - How to Jump to Application
2011-05-17 4:03 AM
Hi
How I can jump from the my bootloader to the Application at 0x08004000 My bootloader address (0x08000000 - 0x0800Cfff ) I tried typedef void (*JUMP_TO)(void); static unsigned int start_adr=0x08000000;// Main code start address void JumpToStart(void) { JUMP_TO go_entry; go_entry = (JUMP_TO) (start_adr); // Jump to Zero Reset go_entry(); } But failed Thanks Arie2011-05-17 4:03 AM
i assume you found bootloading examples floating around the forum
don't forget to setup new interrupt table location for the app you'r etrying to launch from bootloader. (usually done in NVIC init function in examples). Also not sure what toolchain you're using, but in gcc a thing easy to forget is adjusting the linker .ld file hope this will get you going2011-05-17 4:03 AM
i'm not sure that i understand correctly
you have bootloader at 0x08004000 and application at 0x08000000? if yes you can do that in this way: in bootloader: #define BOOTLOADER_APP_ADDR 0x08000000 typedef void (*pFunction)(void); pFunction Jump_To_Application; u32 JumpAddress; //Disable Interupts if you are using it in bootloader app NVIC_DeInit(); //and interrupts which isn't menaged by NVIC and you are using in bootloader app, for egzample sysytick SysTick_ITConfig(DISABLE); JumpAddress = (*(vu32*)(BOOTLOADER_APP_ADDR + 4)); Jump_To_Application = (pFunction) JumpAddress; /* Initialize user application's Stack Pointer */ __MSR_MSP(*(vu32*) BOOTLOADER_APP_ADDR); Jump_To_Application(); in application don't forget: NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x8000000);2011-05-17 4:03 AM
''i assume you found bootloading examples floating around the forum''
please can you tell me where I'd like to see it?2011-05-17 4:03 AM
This may not be what you are looking for but I will give it a shot.
The bootloader should be separate from your application. The ROM reset vector points to your bootloader. The bootloader’s job begins mostly by jumping to your application’s start. Use interrupt slot 7 at 0x1C (it’s “reserved�) for your application start. If your boot loader is to run and uses interrupts put your vector in RAM or if you have space relocate the vectors to your bootloader program space. After the boot loader runs you have 2 choices. Die and wait for an external reset. Or make the processor reset (deadman timer perhaps) to start the just loaded application.