cancel
Showing results for 
Search instead for 
Did you mean: 

SDRAM - Winbond W9825GKH-6l - DMA Access

MMARI.1
Senior II

hi

1. STM32F722ZE & Winbond SDRAM is working fine with follow setting .

W9825G6KH-6I 166MHz/CL3 or 133MHz/CL2   

CASLatency = FMC_SDRAM_CAS_LATENCY_3;

SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_3;

my understanding was MCU main clock was divide by 2 is made on below .

Initially  i kept the SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2; but it's not working then i changed to SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_3; and then it's started working . 

i). what is exact speed now SDRAM is working 108Mhz or 72Mhz ?. 

ii). Initially i calculated  the  timing by 216Mhz/2 = 108Mhz = 9.26ns . should i need change the timing according to 72Mhz .??

iii) what is role of 166MHz/CL3 or 133MHz/CL2 ??.

 

 

 

2. SDRAM is working perfectly by HAL_SDRAM _read.

    How to handle SDRAM by DMA access specifically  DMA _Read .

 

 

#define SDRAM_ADD_1 0xC0000000
#define SDRAM_ADD_2 0xC0000060

 

 

i). i enabled the DMA mem to mem with word (source and destination )and then started DMA by below .

 

 

 HAL_DMA_Start(&hdma_memtomem_dma2_stream0, (uint32_t)SDRAM_ADD_1, (uint32_t)rdata,10);
 HAL_DMA_Start(&hdma_memtomem_dma2_stream1, (uint32_t)SDRAM_ADD_2, (uint32_t)rdata,10);

 

 

accessed DMA by 

 

 

HAL_SDRAM_Read_DMA(&hsdram1, (uint32_t*)SDRAM_ADD_1, (uint32_t*)rdata, 10);
HAL_Delay(1000);
HAL_SDRAM_Read_DMA(&hsdram1, (uint32_t*)SDRAM_ADD_2, (uint32_t*)rdata, 10);

 

 

 

but stream0 is not working from address 1

      stream1 is not working from address 2 .

i need access the  SDRAM address randomly , so i need change the HAL_DMA_Start every time ?.

i think i am not  approaching DMA properly . please suggest me how to approach SDRAM - DMA_Read with random address access 

 

 

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

Not sure what the problem is and what do you mean by


@MMARI.1 wrote:

but stream0 is not working from address 1

      stream1 is not working from address 2 . 

The data written is not read back correctly?

But from this statement, I understand you can read the SDRAM using the CPU but not with DMA but you didn't mention what the problem is? uncorrect data? always 0? or what?

 


@MMARI.1 wrote:

2. SDRAM is working perfectly by HAL_SDRAM _read.

    How to handle SDRAM by DMA access specifically  DMA _Read .

#define SDRAM_ADD_1 0xC0000000
#define SDRAM_ADD_2 0xC0000060

To me, if you are reading perfectly the data by writing and reading them back using the CPU it deas mean your FMC config is good.

Now I'm wondering if you are taking care of the cache coherency as you are transferring the data and reading them back using the CPU! refer to the AN4839 Level 1 cache on STM32F7 Series and STM32H7 Series/ 3.2 Example for cache maintenance and data coherency

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
mƎALLEm
ST Employee

Hello,

Not sure what the problem is and what do you mean by


@MMARI.1 wrote:

but stream0 is not working from address 1

      stream1 is not working from address 2 . 

The data written is not read back correctly?

But from this statement, I understand you can read the SDRAM using the CPU but not with DMA but you didn't mention what the problem is? uncorrect data? always 0? or what?

 


@MMARI.1 wrote:

2. SDRAM is working perfectly by HAL_SDRAM _read.

    How to handle SDRAM by DMA access specifically  DMA _Read .

#define SDRAM_ADD_1 0xC0000000
#define SDRAM_ADD_2 0xC0000060

To me, if you are reading perfectly the data by writing and reading them back using the CPU it deas mean your FMC config is good.

Now I'm wondering if you are taking care of the cache coherency as you are transferring the data and reading them back using the CPU! refer to the AN4839 Level 1 cache on STM32F7 Series and STM32H7 Series/ 3.2 Example for cache maintenance and data coherency

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Probably cache coherency, the debugger sees what the MCU returns and that might not reflect memory content if changed by hardware.

The pins and board wiring may not sustain the higher speeds.

The slower speed and RAS/CAS timing can be more accommodating. Yes you should be able to adjust other timings provided they still meet minimum requirements. Some of the integer divisions might force slower times as the granularity expands as frequency drops,  but min timings are fixed and still need to be met.

Caching can hide much of this, especially as SDRAM have relatively high latency to get the first bytes out, subsequent ones being far less expensive. So well suited to cache line fills.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@mƎALLEm @Tesla DeLorean 

Hi,

Problem is with the  DMA incorrect data is coming and Without the  DMA is working properly .

I do agree with MCU  pins (Nucleo Board) and SDRAM PCB pins connected via the  jumper wire might be cause.

at this movement my question is Will the external  SDRAM work with DMA mode in the  F7 series  DISCOVERY Boards ?.   

One more question that how Touch GFX  using an external SDRAM as buffer in Normal Mode or DMA mode ?.

 

 

Hi @MMARI.1 ,


@MMARI.1 wrote:

at this movement my question is Will the external  SDRAM work with DMA mode in the  F7 series  DISCOVERY Boards ?.   


I don't see how it's something related to the board. DMA works in the same way whatever the F7. 

 

One more question that how Touch GFX  using an external SDRAM as buffer in Normal Mode or DMA mode ?.


For TouchGFX, I kindly invite you to open a new thread in TouchGFX forum, TouchGFX team may help you.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

hi,

I don't have the Discovery board but the SDRAM looks near to the MCU in the discovery board .

If the SDRAM works with the  DMA mode in the Discovery Board then  i need to make own pcb or i need buy the discovery board . 

 

Hello,


@MMARI.1 wrote:

I don't have the Discovery board but the SDRAM looks near to the MCU in the discovery board .

If the SDRAM works with the  DMA mode in the Discovery Board then  i need to make own pcb or i need buy the discovery board . 


Sorry didn't understand. The statement is not clear. 

Also, what discovery board you are referring to? As you are talking about STM32F722 (in the original post), the only DISCO board compatible is the STM32F723E-Discovery that doesn't have SDRAM but PSRAM.

PS: I unselected the "Accept as Solution"

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.