cancel
Showing results for 
Search instead for 
Did you mean: 

SDRAM HAL_SDRAM_WRITE_32b function not working for stm32H7.

Aarra.1
Senior

Hello,

I'm using STM32H757i-EVAL board and trying to store some data in the onboard SDRAM using stm32cubeide (1.7.0).

Below is my initialization for SDRAM

void MX_FMC_Init(void)
{
 
  /* USER CODE BEGIN FMC_Init 0 */
 
  /* USER CODE END FMC_Init 0 */
 
  FMC_SDRAM_TimingTypeDef SdramTiming = {0};
 
  /* USER CODE BEGIN FMC_Init 1 */
 
  /* USER CODE END FMC_Init 1 */
 
  /** Perform the SDRAM1 memory initialization sequence
  */
  hsdram1.Instance = FMC_SDRAM_DEVICE;
  /* hsdram1.Init */
  hsdram1.Init.SDBank = FMC_SDRAM_BANK2;
  hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_8;
  hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12;
  hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_32;
  hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;
  hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_1;
  hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
  hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_DISABLE;
  hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_DISABLE;
  hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_0;
  /* SdramTiming */
  SdramTiming.LoadToActiveDelay = 2;
  SdramTiming.ExitSelfRefreshDelay = 6;
  SdramTiming.SelfRefreshTime = 4;
  SdramTiming.RowCycleDelay = 6;
  SdramTiming.WriteRecoveryTime = 2;
  SdramTiming.RPDelay = 2;
  SdramTiming.RCDDelay = 2;
 
  if (HAL_SDRAM_Init(&hsdram1, &SdramTiming) != HAL_OK)
  {
    Error_Handler( );
  }
 
  /* USER CODE BEGIN FMC_Init 2 */
 
  /* USER CODE END FMC_Init 2 */
}
static void SDRAM_Initialization_Sequence(SDRAM_HandleTypeDef *hsdram)
{
  FMC_SDRAM_CommandTypeDef Command={0};
 
  __IO uint32_t tmpmrd =0;
  /* Step 1:  Configure a clock configuration enable command */
  Command.CommandMode = FMC_SDRAM_CMD_CLK_ENABLE;
  Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1; //FMC_SDRAM_CMD_TARGET_BANK1
  Command.AutoRefreshNumber = 1;
  Command.ModeRegisterDefinition = 0;
 
  /* Send the command */
  HAL_SDRAM_SendCommand(hsdram, &Command, SDRAM_TIMEOUT);
  HAL_Delay(1);
 
  /* Step 3: Configure a PALL (precharge all) command */
  Command.CommandMode = FMC_SDRAM_CMD_PALL;
  Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1;
  Command.AutoRefreshNumber = 1;
  Command.ModeRegisterDefinition = 0;
 
  /* Send the command */
  HAL_SDRAM_SendCommand(hsdram, &Command, SDRAM_TIMEOUT);
 
  /* Step 4 : Configure a Auto-Refresh command */
  Command.CommandMode = FMC_SDRAM_CMD_AUTOREFRESH_MODE;
  Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1;
  Command.AutoRefreshNumber = 8;
  Command.ModeRegisterDefinition = 0;
 
  /* Send the command */
  HAL_SDRAM_SendCommand(hsdram, &Command, SDRAM_TIMEOUT);
 
 
  /* Step 5: Program the external memory mode register */
  tmpmrd = (uint32_t)SDRAM_MODEREG_BURST_LENGTH_1          |
                     SDRAM_MODEREG_BURST_TYPE_SEQUENTIAL   |
                     SDRAM_MODEREG_CAS_LATENCY_3           |
                     SDRAM_MODEREG_OPERATING_MODE_STANDARD |
                     SDRAM_MODEREG_WRITEBURST_MODE_SINGLE;
 
  Command.CommandMode = FMC_SDRAM_CMD_LOAD_MODE;
  Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1;
  Command.AutoRefreshNumber = 1;
  Command.ModeRegisterDefinition = tmpmrd;
 
  /* Send the command */
  HAL_SDRAM_SendCommand(hsdram, &Command, SDRAM_TIMEOUT);
 
  /* Step 6: Set the refresh rate counter */
  /* Set the device refresh rate */
  HAL_SDRAM_ProgramRefreshRate(hsdram, REFRESH_COUNT);
 
}

I'm using HAL_SDRAM_Write_32b function to write some data into the SDRAM.

While I'm passing the address variable, the address is being updated to some other junk value and the data is not being written into the desired address.

I have tried all means to configure the same.

Kindly help me find the solution for the same.

Regards.

1 REPLY 1
Aarra.1
Senior

kindly help me with this problem.