2018-11-14 07:39 AM
Hi,
I am using the IDW04A1 WiFi module for a project where I want to transfer potentially large files to a server. Is there a way of accessing the SD slot from my MCU?
I am using the STM32F401RE MCU and currently I use an external SD to save files. If I can access the on board SD card slot that would make things a lot simpler.
Thanks
2018-11-19 04:41 AM
Hi,
you several way to transfer files from/to the SD card:
The SD card is also accessible through the on board http(s) server.
Does this answer your question?
Regards,
Elio