2015-02-13 04:19 AM
Hi
It was not clear from the datasheet, but is the TAMPFREQ register only applicable when using level detection and not edge detection?I am asking as PC13 (RTC_TS) is not available on some low pin count packages and was thinking RTC_TAMP2 with TAMPTS set could work.Thanksleppie #rtc-tamper-timestamp2015-02-17 02:06 AM
Anyone?
2015-02-19 08:58 PM
From some testing, it would seem TAMPFREQ does not have an effect when using edge triggering.