cancel
Showing results for 
Search instead for 
Did you mean: 

RTC on Timer Interrupts

meena
Associate III

I am using TIMER 14 for counting test durations in my projects however I am lagging off aroumd 5 mins per week.How can i implement the same with RTC counter?

1 REPLY 1
Techn
Senior II

The accuracy depends on the crystal. If you really need very accurate timing, adjust the timer reload value or use external rtc such as ds3231 which can generate 1 sec pulse use it to.generate interrupt and do the counting.