reseting STSPIN32G4
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-01-19 3:13 PM - edited 2024-01-19 3:22 PM
Hello!
I’ve been working with STSPIN32G4 for while with low voltage (9V), it works good
I set 24V and have problems with nFaults, it being set, meaning that driver is turned off, although no fault is indicated, status register: 10001000
D3 Indicates if the registers had been reset to the default (power-up)
D2, D1, D0 - VDS_P, THSD, VCC_UVLO
black ones are extra 10uF electrolytic capacitors
Vcc=8V DC
VDD = 3,3V DC
What can be wrong or what else should i check?
Labels:
- Labels:
-
STM32G4 series
0 REPLIES 0