cancel
Showing results for 
Search instead for 
Did you mean: 

Reset pin Status

bsuthar
Associate II

Hello team,

Generally , Reset pin by default status is Logic High.

But in AN4206 ( Page 31) , NRST pin is not Connected to 3.3V , it is left Floating with Capacitor.

Is that Okay ? 

My device is STM32F303.

Regards,

1 REPLY 1
TDK
Super User

Yes, the typical connection is floating with 0.1 uF cap. It is internally pulled up.

TDK_0-1754142734193.png

 

If you feel a post has answered your question, please click "Accept as Solution".