cancel
Showing results for 
Search instead for 
Did you mean: 

Application excecusion issue while jumping (SDRAM)

Vishwajeet
Associate II


Hello,

I am working on an STM32F746 project where I have implemented a bootloader.
The setup is as follows:

Application image is stored in external QSPI flash.

Bootloader copies the image from QSPI to SDRAM (IS42S32400F at 0xC0000000).

After copying, I set SCB->VTOR = 0xC0000000 and jump to the application Reset_Handler.

The copy is verified: I have cross-checked the SDRAM contents with the QSPI image, and the data is copied correctly.

I also created a test application that only sets a GPIO pin high (no SystemInit(), no HAL_Init(), no HAL_RCC_DeInit()).
Even in this simple case, after the bootloader jumps to the reset handler, I get this error:

 


Break at address "0x242" with no debug information available, or outside of program code.

The Reset_Handler address from the SDRAM vector table is correct (e.g., 0xC00002B5), and VTOR is updated to 0xC0000000.
But execution always ends up breaking at 0x242.

Has anyone faced this issue when trying to execute code from SDRAM after copying from QSPI?
Any hints on what I might be missing (cache setup, MPU, remap, or SDRAM execution settings)?

Thanks in advance.

8 REPLIES 8
mƎALLEm
ST Employee

Hello,

First test to do is to disable the cache.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Kindly review my jump function .

thank you

void VerifyAndJumpOrDump(uint32_t app_size)

{

uint32_t v0 = *(volatile uint32_t*)(APP_BASE + 0);

uint32_t v1 = *(volatile uint32_t*)(APP_BASE + 4);





SCB->VTOR = APP_BASE;



print_hex("VTOR (should be APP_BASE) ", SCB->VTOR);

print_hex("Vector[0] (SP) at APP_BASE ", v0);

print_hex("Vector[1] (PC) at APP_BASE ", v1);



if (!is_valid_sp(v0)) {

printf("Invalid SP at APP_BASE! scanning SDRAM for vector table...\r\n");



int32_t found_offset = scan_for_vector_table(0x10000); // scan first 64KB

if (found_offset >= 0) {

printf("Found candidate vector at APP_BASE + 0x%X\r\n", found_offset);

dump_memory_hex(APP_BASE + found_offset, 8);

} else {

printf("No plausible vector found in first 64KB of SDRAM.\r\n");

}



// Dump first 16 words at APP_BASE to help debug

dump_memory_hex(APP_BASE, 16);

while (1) { HAL_Delay(1000); } // halt for debug

}



// SP looks valid, check PC

if (!is_valid_pc(v1)) {

printf("PC looks invalid (not in flash or SDRAM). Dumping memory near APP_BASE...\r\n");

dump_memory_hex(APP_BASE, 32);

while (1) { HAL_Delay(1000); } // halt for debug

}



// ensure Thumb bit in PC

if ((v1 & 0x1U) == 0) {

printf("PC LSB (Thumb bit) is NOT set! Forcing Thumb bit for jump, but image may be wrong.\r\n");

}



// Optional: configure MPU so SDRAM is executable (call only if using MPU)

// MPU_Config_SDRAM_Executable();



// Clean D-cache for the app area (aligned to 32 bytes)

uint32_t start = APP_BASE & ~0x1FU;

uint32_t end = (APP_BASE + app_size + 31) & ~0x1FU;

uint32_t size = end - start;

printf("Cleaning D-Cache for 0x%08X - 0x%08X (size 0x%X)\r\n", start, end, size);

// SCB_CleanInvalidateDCache_by_Addr((uint32_t*)start, size);

// SCB_InvalidateICache();

__DSB(); __ISB();



// Disable interrupts, stop SysTick, clear pending/enable bits

__disable_irq();

SysTick->CTRL = 0;

for (int i = 0; i < 8; i++) {

NVIC->ICPR[i] = 0xFFFFFFFF;

NVIC->ICER[i] = 0xFFFFFFFF;

}



// Set VTOR (redundant if already set but safe)

SCB->VTOR = APP_BASE;

__DSB(); __ISB();



// Set MSP then jump

__set_MSP(v0);

__DSB(); __ISB();



pFunction Jump = (pFunction)(v1 | 0x1U); // ensure Thumb bit set

printf("Jumping to 0x%08X (Thumb)\r\n", (unsigned)(v1 & ~1U));

Jump();



// should not return

while (1);

}

If your solution is not solved why did you accept the solution?

In next time please use </> button to insert your code. Please read this post.

I'm editing your post then.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Vishwajeet
Associate II

I am really sorry kindly continue this topic 

Did you try to disable the cache or not?

The closest example I can find (it's for H7) is the Template example ExtMem_Boot:

https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H750B-DK/Templates/ExtMem_Boot

It can execute the code from SDRAM after copying the binary from an external memory (QSPI for example).

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Ozone
Principal III

> I also created a test application that only sets a GPIO pin high (no SystemInit(), no HAL_Init(), no HAL_RCC_DeInit()).

I don't know your board, but the SDRAM is external, I think.
Check the respective initialisation for the external memory bus peripheral is executed, either in the startup code or (more likely) in SystemInit().
Without initialising the bus interface, code execution from this RAM inevitably crashes.

Hello @Vishwajeet 

Please refer to the AN5188.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om

Hello ,

 

https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H750B-DK/Templates/ExtMem_Boot

 

I tried the example configuration for relocating code to SDRAM, but I face HardFaults in both cases:

If I disable caches (I-Cache and D-Cache):
→ The CPU goes into HardFault immediately.

If I enable caches:
→ The CPU still ends up in HardFault when trying to jump to the SDRAM application.

 

i have attached memory snap Below