2023-11-02 11:26 PM
Hi!
Can you recommend me a suitable usb driver to connect STM32H735VGH in device mode ?
And please suggest me if any additional configuration required to work with.
Thank you.
2023-11-05 12:14 PM
Hello @shaktipg and welcome to the ST Community
I suggest you take a look at the USB_Device examples for the STM32H735G-DK board as a start for your project.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.