Skip to main content
Associate III
April 27, 2025
Question

Counting Six External Pulse Inputs Using Timers on STM32U575ZIT6Q

  • April 27, 2025
  • 2 replies
  • 524 views

Hi Support Team,

I am currently using the STM32U575ZIT6Q MCU for development.
As per our project requirements, I need to count six independent external pulse signals (from a wind-turbine RPM sensor or similar) with a maximum frequency of approximately 100 kHz.
The counter is expected to roll over naturally and reset upon system reboot (final hardware will use the STM32U585 series).

Here are my observations and concerns:
1. I had previously raised a similar query.
2. Could you please guide me on how to configure the timers to count at least six independent external inputs?
3. As per STM32CubeMX, the STM32U575ZIT6Q provides only 5 timers supporting ETR pins for external clock input.
4. I have observed that enabling certain configurations in Slave Mode disables other options like Trigger Source,
Clock Source, and Channel Configurations, leading to conflicts.
5. Could you suggest an alternative method to count six external pulse inputs? (Either using different channels or Interrupt, DMA method)

If possible, could you please share recommended STM32CubeMX configurations and/or example firmware code for this use case? Along with this I have attached a code of sample which I am usi

static void MX_TIM3_Init(void)
{

 /* USER CODE BEGIN TIM3_Init 0 */

 /* USER CODE END TIM3_Init 0 */

 TIM_SlaveConfigTypeDef sSlaveConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};

 /* USER CODE BEGIN TIM3_Init 1 */

 /* USER CODE END TIM3_Init 1 */
 htim3.Instance = TIM3;
 htim3.Init.Prescaler = 0;
 htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim3.Init.Period = 4294967295;
 htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
 if (HAL_TIM_Base_Init(&htim3) != HAL_OK)
 {
 Error_Handler();
 }
 sSlaveConfig.SlaveMode = TIM_SLAVEMODE_EXTERNAL1;
 sSlaveConfig.InputTrigger = TIM_TS_ETRF;
 sSlaveConfig.TriggerPolarity = TIM_TRIGGERPOLARITY_NONINVERTED;
 sSlaveConfig.TriggerPrescaler = TIM_TRIGGERPRESCALER_DIV1;
 sSlaveConfig.TriggerFilter = 0;
 if (HAL_TIM_SlaveConfigSynchro(&htim3, &sSlaveConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_ENABLE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM3_Init 2 */

 /* USER CODE END TIM3_Init 2 */

}

void Timer_Handling_Thread(void *argument)
{
	char iridium_buffer[64] = {0};
	HAL_TIM_Base_Start(&htim5);
	while(1)
	{
		uint32_t count = __HAL_TIM_GET_COUNTER(&htim5);
		snprintf(iridium_buffer, sizeof(iridium_buffer),"Pulse Count: %lu (dec), 0x%lX (hex)\r\n", count, count);
		HAL_UART_Transmit(&huart2, (uint8_t *)iridium_buffer, strlen(iridium_buffer), HAL_MAX_DELAY);
	}
}

ng.

Your guidance would be very helpful as this directly impacts our hardware pin planning and overall system design.

Waiting for your response.

Thanks and Regards,
Ramesh

This topic has been closed for replies.

2 replies

TDK
April 27, 2025
"If you feel a post has answered your question, please click ""Accept as Solution""."
ram_janAuthor
Associate III
April 28, 2025

Hi Team,

Could you please help by sharing the STM32 CubeMX configurations needed to implement the above-mentioned functionality?
If possible, it would be great if you could also share a working firmware example.

Here are a few specific queries:
1. Is it possible to count pulses from six external inputs simultaneously?
2. Could you please suggest the most appropriate slave method to implement this?
3. Why are some configurations getting disabled when changes are made to the Slave Mode settings?
4. If using DMA is a suitable solution, could you please provide a reference example or the related CubeMX settings?

Note: I am currently using STM32 CubeIDE version 1.18.0 for development.

Thanks,