2022-07-31 10:33 AM
I would like to change the stm32l476rgt6 to the stm32l476ret6 , in general they are the same MCU changing only the amount of flash memory (1Mb to 512k), is there any problem? remembering that I have a project already running with rgt6.
in general I think I would just need to change the Script linker, but I would like to rectify this idea.
Thanks.
2022-08-01 03:30 AM
Hi @KSilv.1 and welcome to STM32 Community ,
If your project is based on a generation of code with STM32CubeMX, this article can help you to migrate your current STM32L476RGT6 example to the STM32L476RET6.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.