cancel
Showing results for 
Search instead for 
Did you mean: 

Replacement for LPC1764FBD100

Chaitanya1
Associate II

We are looking for a replacement of NXP microcontroller LPC1764FBD100. Can you please suggest a suitable ST Microcontroller?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Depending on your specific requirements, there are many STM32 that could be used instead of the LPC1764FBD100. However, it should be noted that no pin-compatible is possible, so a new circuit and a rewrite of the programme are necessary.

You can, however, look at, for example:

Hope that helps?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Foued_KH
ST Employee

Hello @Chaitanya​ ,

It offers products combining very high performance, real-time capabilities, digital signal processing, low-power / low-voltage operation, and connectivity, while maintaining full integration and ease of development.It offers products combining very high performance, real-time capabilities, digital signal processing, low-power / low-voltage operation, and connectivity, while maintaining full integration and ease of development.

0693W00000bhUhsQAE.jpg 

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Chaitanya1
Associate II

Hi @KHALSI_Foued​ ,

I guess, you have missed to suggest the alternate part.

Peter BENSCH
ST Employee

Depending on your specific requirements, there are many STM32 that could be used instead of the LPC1764FBD100. However, it should be noted that no pin-compatible is possible, so a new circuit and a rewrite of the programme are necessary.

You can, however, look at, for example:

Hope that helps?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Chaitanya1
Associate II

Thanks @Peter BENSCH​ . I will check the suggested parts.