cancel
Showing results for 
Search instead for 
Did you mean: 

Regulator in Range 2. RM0444

Xme
Associate II

Xme_4-1744645822286.png

 

 

Xme_3-1744645756472.png

 

Xme_5-1744645960865.png

 

Xme_6-1744646115679.png

 

 

Where is the truth ?

 

 

4 REPLIES 4
TDK
Super User

Both. They're talking about different things. "Range 2" is not "low-power run mode".

If you feel a post has answered your question, please click "Accept as Solution".

@TDK wrote:

 "Range 2" is not "low-power run mode".


Indeed.

@Xme - more details of what regulators are used in which power modes here:

AndrewNeil_0-1744649669639.png

and here:

AndrewNeil_1-1744649742089.png

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Xme
Associate II

So what is difference? 

it means that when I change voltage scaling to Range 2 while program runs, HCLK can be max 16Mhz .

But when after this I want use WFI(),  the HCLK must be 2MHz max ?

TDK
Super User

The MCU can be clocked from the normal regular (range 1 or range 2) or the low-power regulator (low power run mode).

Low-power run mode is a lower power consumption mode than either range 1 or range 2.

TDK_0-1744722571628.png

 

If you feel a post has answered your question, please click "Accept as Solution".