cancel
Showing results for 
Search instead for 
Did you mean: 

Regarding issue with NUCLEO-F429ZI.

sadvik_reddy
Associate

NUCELO-F429ZI Encountered a issue.

When i connect a USB ,it is showing like FAIL and a message is shown on the screen like

The interface firmware FAILED to reset/halt the target MCU.

Can any one let me know what is the reason for this and solution for this.

3 REPLIES 3
AScha.3
Chief III

Try with CubeProgrammer , set mode "under reset" , reset "hardware reset" , connect ;

then show , what it tells (screenshot).

If you feel a post has answered your question, please click "Accept as Solution".

Screenshot (56).png

see:

AScha3_0-1714036311799.png

So your board -> F429 cpu has no power.  Check jumper settings, see board manual.

Then connect again....

If you feel a post has answered your question, please click "Accept as Solution".