cancel
Showing results for 
Search instead for 
Did you mean: 

Realtime SWV debugging

hesam moshiri
Associate III

I have enabled an ADC of a STM32F407. I want to check how well it samples the input signal, therefore I should see in in the SWV graph.

But it seems the SWV is unable to grab all data sequentially. I read ADC using DMA and 1000 buffer length.

How can I fix this limitation?

1 REPLY 1
T J
Lead

I print to the serial port at 230400baud,

to show data on a static display

every 100mS

setCursor( row,Column) ; // check VT100 commands

print A/Ds and "clear to end of line", "<esc>[0K" to clean up any old overprint