cancel
Showing results for 
Search instead for 
Did you mean: 

reading I/O register values with command line GDB

M. Jeong
Associate II
Posted on December 18, 2017 at 16:54

Recently I found that STM32CubeMX support Makefile as well as SW4STM32. So far I worked with only the SW4STM32, but now I'm happy to move to the command line development with GCC, GNU make , stlink, and GDB. After spending time fixing minor bugs I could compile a blinky code and flashed my STM32L476 without problem. The blinky program is working as expected. 

Now I'm trying to debug the program with GDB. I ran st-util and arm-none-eabi-gdb using my .elf file. Then setting breakpoints and reading the values of variables were successful. But I wonder how to read I/O register values. On the System Workbench for STM32 it's very easy to check the state of the I/O registers. Would it be possible for one to do the same thing on the command line? For example, how can you read the values of GPIOB_MODER, GPIOB_OTYPER, and GPIOB_ODR registers at once?

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
waclawek.jan
Super User
Posted on December 18, 2017 at 17:02

Use -g3 when compiling, the compiler then adds macros into debug info.

Then in gdb simply type p /x *GPIOB

Enjoy! ;)

JW

Posted on December 18, 2017 at 17:13

Hi JW,

thank you for the quick answer! The flag '-g3' worked. This is awesome.. I feel like I don't need the heavy IDE anymore.

I have two questions. Is there a command which displays the register values in binary format? Would it be bad that one uses the -g3 option to compile a release version(for flashing)?

thanks

Posted on December 18, 2017 at 17:23

Is there a command which displays the register values in binary format?

Use /t modifier instead of /x in p (print) command. The result is IMO less readable than hexadecimal.

Compare

(gdb) p /t TIM3->CCMR1

$39 = 1111000111110001

(gdb) p /x TIM3->CCMR1

$40 = 0xf1f1

Would it be bad that one uses the -g3 option to compile a release version(for flashing)?

Shouldn't matter, as -g3 should influence only the debug information, which does not go to the binary for FLASH.

JW

Posted on December 21, 2017 at 08:42

Hi JW,

with the -g3 flag I could debug my program for STM32L476-discovery board. But strangely I cannot read I/O registers of STM32F407 using the flag. When the source code is compiled by SW4STM32, then command line gdb shows the I/O register values. However, when it's compiled using

https://github.com/nownuri/STM32F407_command_line_development/blob/master/STM32F407_make/Makefile

, the gdb says 'no symbol 'RCC' in current context'. The Makefile is almost same as the one worked well for my STM32L4. I tried various flags (-O0/-Og/-O and -g/-ggdb/-g3), but I couldn't solve the problem. 

Could you please have a look at my Makefile linked above, or could you please post your one?

Thank you,

Posted on December 21, 2017 at 09:35

Reading makefiles is no fun. Look at the command line the makefile produces. Can't there be multiple conflicting -g in it?

JW

Posted on January 22, 2018 at 17:50

Unfortunately I still couldn't success with STM32F4Discovery. The following is the Makefile setting which is relevant to the debugging. To me this looks just fine, but it doesn't allow gdb to read register values. Symbols like GPIOD are not found in gdb.

     ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯

      ♯ building variables

      â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯â™¯

      â™¯ debug build?

      DEBUG = 1

      â™¯ optimization

      OPT = -Og

      â™¯ compile gcc flags

      ASFLAGS = $(MCU) $(AS_DEFS) $(AS_INCLUDES) $(OPT) -Wall -fdata-sections -ffunction-sections

      CFLAGS = $(MCU) $(C_DEFS) $(C_INCLUDES) $(OPT) -Wall -fdata-sections -ffunction-sections

      ifeq ($(DEBUG), 1)

      CFLAGS += -g3 -gdwarf-2

      endif
Posted on January 22, 2018 at 19:57

As I've said above,

Reading makefiles is no fun. Look at the command line the makefile produces

You also can check if the .elf contains the macros, using arm-none-eabi-objdump --dwarf=macro xxxx.elf >xxxx.dwarf

JW