2024-01-13 12:32 AM - edited 2024-01-13 12:32 AM
I am working on STM32F407ZET6 with DMA+SPI in slave mode. Trying to reset DMA Counter when NSS is high to avoid shifted data transmit.
TX and RX DMA are working on Circular mode.
This is my tx data
typedef struct {
uint8_t InputState[4];
uint8_t reserved1[4];
uint8_t reserved2[4];
uint8_t reserved3[4];
} SyncDataTX;
Inside init function, i did
*((uint32_t*)(txData.InputState)) = 0x11121314;
*((uint32_t*)(txData.reserved1)) = 0x15161718;
*((uint32_t*)(txData.reserved2)) = 0x19202122;
*((uint32_t*)(txData.reserved3)) = 0x23242526;
HAL_SPI_TransmitReceive_DMA(&hspi1, (uint8_t *)&txData, (uint8_t *)&rxData, sizeof(txData));
Inside interrupt function, i did
__HAL_DMA_DISABLE(&hdma_spi1_rx);
__HAL_DMA_DISABLE(&hdma_spi1_tx);
__HAL_DMA_SET_COUNTER(&hdma_spi1_rx,sizeof(SyncDataTX));
__HAL_DMA_SET_COUNTER(&hdma_spi1_tx,sizeof(SyncDataTX));
__HAL_DMA_ENABLE(&hdma_spi1_rx);
__HAL_DMA_ENABLE(&hdma_spi1_tx);
In the first transaction, I get this, which is correct data:
11121314
15161718
19202122
23242526
In the second transaction, I get this:
12131414
16171811
20212215
24252619
From the third transaction, I start to getting this:
12131423
16171811
20212215
24252619
This happens even only:
__HAL_DMA_DISABLE(&hdma_spi1_tx);
__HAL_DMA_ENABLE(&hdma_spi1_tx);
🤔I didn't encounter such problem in STM32H750
Solved! Go to Solution.
2024-01-13 09:38 PM - edited 2024-01-13 09:51 PM
this makes sense. I will try your solution.
But I'm still confused that why the problem is still there even only do this
__HAL_DMA_DISABLE(&hdma_spi1_tx);
__HAL_DMA_ENABLE(&hdma_spi1_tx);
2024-01-13 10:02 PM - edited 2024-01-13 10:06 PM
I was thinking that DMA starts to transfer data to DR only when NSS is low 🤔 which was wrong.
It seems that DMA starts to transfer data to DR when DR is empty
Actually there's no need to stop and restart SPI. My solution is overwriting the first byte in DR, and let DMA transfer the remaining bytes ( startPointer+1 to totalLength-1 )
__HAL_DMA_DISABLE(&hdma_spi1_tx);
__HAL_DMA_SET_COUNTER(&hdma_spi1_tx,SyncSize-1);
(&hspi1)->Instance->DR = *((uint8_t*)((&hspi1)->pTxBuffPtr));
(&hdma_spi1_tx)->Instance->M0AR = (uint32_t)((&hspi1)->pTxBuffPtr+1);
__HAL_DMA_ENABLE(&hdma_spi1_tx);
Thanks for help. :D