Skip to main content
wan512
Associate II
December 5, 2014
Solved

[question] can I disable the nucleo onboard stlink mass-storage?

  • December 5, 2014
  • 3 replies
  • 1887 views
Posted on December 05, 2014 at 10:05

i'v tested the nucleo on arm mbed, very nice.

but, when i use the onboard stlink v2.1 to debug my application board, the mbed mass-storeage disk is always pop-up a window.

so, can i disable this disk (not by disbable the system autorun function), only keep the stlink swd & cdc functions?

#nucleo-f401re-st-link/v2-1
    Best answer by mƎALLEm

    Hello,

    As said by @Andrew Neil , you can disable it by changing type but you can do it with CubeProgrammer:

    Click "Firmware upgrade button" Then click "Open in update mode" button. Check the box "Change type" , finally select "STM32 Debug+VCP" and click "Update": 

    SofLit_0-1706708891249.png

     

     

    3 replies

    Andrew Neil
    Super User
    January 31, 2024

    I also had this question, and a forum search found this unanswered post.

    I load code direct from the IDE - I don't use the mass storage - so the pop-up of the file explorer window is just a nuisance.

    Turns out there is a way to disable the mass storage feature of the ST-Links on Nucleo boards:

    https://community.st.com/t5/stm32-mcus-boards-and-hardware/st-link-on-nucleo-boards-without-connecting-an-usb-memory-device/m-p/191920

    it uses the ST-Link Updater, STSW-LINK007https://www.st.com/en/development-tools/stsw-link007.html 

    That gives you the option to change the 'Type' from 'Debug + Mass Storage + VCP' to just 'Debug + VCP' 

    AndrewNeil_0-1706705682018.png

     

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    mƎALLEm
    mƎALLEmBest answer
    ST Technical Moderator
    January 31, 2024

    Hello,

    As said by @Andrew Neil , you can disable it by changing type but you can do it with CubeProgrammer:

    Click "Firmware upgrade button" Then click "Open in update mode" button. Check the box "Change type" , finally select "STM32 Debug+VCP" and click "Update": 

    SofLit_0-1706708891249.png

     

     

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
    Pavel A.
    January 31, 2024

    Another easy way, even without touching the ST-LINK firmware: open Device Manager and disable the disk device associated with the ST-LINK. If you have only one or few boards or ST-LINKs, this is the easiest and safest method.