2018-05-28 11:53 PM
Dear STM Community,
we want to use I2C in Fast Mode Plus (1MBit/s) with a STM32F401xB MCU. The datasheet points out: 'The I2C bus
frequency can be increased up to 1 MHz.' What are the conditions and requirements to implement the pointed out solution? Can I update my in field MCUs with that feature?I'm looking forward to your answer.Kind Regards
Oliver
#stm32f401 #i2c-datasheet #i2c-setup2018-05-29 02:15 AM
Hello
oliver.richter
,As noted in the
STM32F401
datasheet, please contact yourFAE or a local ST sales representative for more details about the complete solution related to I2C fast mode.The I2C bus interface supports standard mode (up to 100 kHz) and fast mode (up to 400 kHz). The I2C bus frequency can be increased up to 1 MHz. For more details about the complete solution, please contact your local ST sales representative.
With Regards,
Imen
2018-05-29 04:08 AM
Can I update my in field MCUs with that feature?
This is only the (supposed) master.
For a successful application, your slave devices and the bus layout must support this clock frequency as well.