2018-05-29 12:40 AM
Hello everybody,
i have a strange problem, hope that someone has a great idea what i can do...
We have custom board's with the stm32f7 and f4. Normaly we flash the device via bat (or open ocd(which is working)).
The bat looks like this:
..\st-link\ST-LINK_CLI.exe -c SWD UR -Rst
..\st-link\ST-LINK_CLI.exe -c SWD UR -P firmware.hex..\st-link\ST-LINK_CLI.exe -c SWD UR -P bootloader.hex..\st-link\ST-LINK_CLI.exe -c SWD UR -Rstpause
Since someday's i get the follow error message while flashing:
The elf loader file is not accessible.
This is the complete output from the console:
ST-LINK SN : 33FF68064D4E353545150843
ST-LINK Firmware version : V2J24S4Connected via SWD.SWD Frequency = 4000K.Target voltage = 3.2 V.Connection mode : Connect Under Reset.Device ID:0x449Device flash Size : 512 KbytesDevice family :STM32F74x/F75xLoading file...
Flash Programming: File : firmware.hex Address : 0x00200000Memory programming...?????????????????????????????????????????????????? 0%The elf loader file is not accessible.We have this problem on two PC's and one PC is working.
I already tried:
Flashing via St-Utility -> Working without a problem
Flashing via openocd ->
Working without a problem
SWD Frequenz to 1800K -> Same problem
Updated St-Utility
-> Same problem
Firmware Update the St-Link
-> Same problem
Take a Brandnew ST-Link
-> Same problem
Updated Win driver
-> Same problem
Taking the st-link from the pc which is working
-> Same problem
What can i do or try?
If you know something i would be very happy
Thank you and have a nice day!
#loader #elf #bat2018-05-29 1:21 AM
Are you sure you are not having spaces in the path name of your ELF file ?
And if so, is the path surrounded by ' - characters ?
2018-05-29 2:08 AM
Yes i'm hundert percent sure.
But you have give me a idea.
I copyd the bat and hex file directly to the st link folder. There It's working. So for me it looks like i have a not acessable file or something like this.
2018-05-29 4:28 AM
Path names in Windows are often not what it seems.
And for certain system paths special restrictions apply, and strange this happen if you try 'normal business' there.
I would switch the batch echo output on, to see the actual path. Perhaps another invalid character.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.