2022-04-15 2:13 AM
Hello, I tried to start QSPI working on a Single flash mode but have a problem with non readable part config registers (NonVolatile, Volatile and Enhanced Volatile). As I understand when working in Dual Flash mode this registers should write and read in pairs, but I receive this weird data(the screen below). In Single flash mode all registers have only 0x55. The question is:
The microcontroller is STM32H750B-DK and external memory MT25QL512ABB
Solved! Go to Solution.
2022-04-15 11:52 AM
The BOARD is STM32H750B-DK, the MCU is STM32H750XBH6
Will come down to initialization code, which you don't show.
The two chips share a common chip select, but the second one is the QSPI BK2 data pins.
You should be able to read a byte if dual mode is disabled, and you use QSPI_FLASH_ID_1
2022-04-15 11:52 AM
The BOARD is STM32H750B-DK, the MCU is STM32H750XBH6
Will come down to initialization code, which you don't show.
The two chips share a common chip select, but the second one is the QSPI BK2 data pins.
You should be able to read a byte if dual mode is disabled, and you use QSPI_FLASH_ID_1
2022-04-18 12:01 AM
This register read is from dual-flash config. This is the initialization code:
void MX_QUADSPI_Init(void)
{
/* USER CODE BEGIN QUADSPI_Init 0 */
/* USER CODE END QUADSPI_Init 0 */
/* USER CODE BEGIN QUADSPI_Init 1 */
/* USER CODE END QUADSPI_Init 1 */
hqspi.Instance = QUADSPI;
hqspi.Init.ClockPrescaler = 1;
hqspi.Init.FifoThreshold = 1;
hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;
hqspi.Init.FlashSize = 19;
hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_4_CYCLE;
hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
//#ifdef FLASHID
// hqspi.Init.FlashID = QSPI_FLASH_ID_1;
//#else
hqspi.Init.FlashID = QSPI_FLASH_ID_1;
//#endif
hqspi.Init.DualFlash = QSPI_DUALFLASH_ENABLE;
if (HAL_QSPI_Init(&hqspi) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN QUADSPI_Init 2 */
/* USER CODE END QUADSPI_Init 2 */
}
void HAL_QSPI_MspInit(QSPI_HandleTypeDef* qspiHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
if(qspiHandle->Instance==QUADSPI)
{
/* USER CODE BEGIN QUADSPI_MspInit 0 */
/* USER CODE END QUADSPI_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_QSPI;
PeriphClkInitStruct.QspiClockSelection = RCC_QSPICLKSOURCE_D1HCLK;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/* QUADSPI clock enable */
__HAL_RCC_QSPI_CLK_ENABLE();
__HAL_RCC_GPIOG_CLK_ENABLE();
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
/**QUADSPI GPIO Configuration
PG6 ------> QUADSPI_BK1_NCS
PF6 ------> QUADSPI_BK1_IO3
PF7 ------> QUADSPI_BK1_IO2
PF10 ------> QUADSPI_CLK
PF9 ------> QUADSPI_BK1_IO1
PD11 ------> QUADSPI_BK1_IO0
*/
GPIO_InitStruct.Pin = GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF10_QUADSPI;
HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF10_QUADSPI;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_11;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/* USER CODE BEGIN QUADSPI_MspInit 1 */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
/**QUADSPI GPIO Configuration
PG9 ------> QUADSPI_BK2_IO2
PG14 ------> QUADSPI_BK2_IO3
PF10 ------> QUADSPI_CLK
PH2 ------> QUADSPI_BK2_IO0
PH3 ------> QUADSPI_BK2_IO1
*/
GPIO_InitStruct.Pin = GPIO_PIN_9|GPIO_PIN_14;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;
HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;
HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);
// Reset the QuadSPI memory interface
__HAL_RCC_QSPI_FORCE_RESET();
__HAL_RCC_QSPI_RELEASE_RESET();
// NVIC configuration for QSPI interrupt
HAL_NVIC_SetPriority(QUADSPI_IRQn, 0x0F, 0);
HAL_NVIC_EnableIRQ(QUADSPI_IRQn);
/* USER CODE END QUADSPI_MspInit 1 */
}
}