2024-01-30 07:25 AM
Hello Everyone
I am try to upload my code through stm32f103 necleo debuger or programmer but have facing one issue for no st link found error
I have attached the pic please give the solution .
2024-01-30 07:55 AM
Hi,
Was the nucleo/st-link working before ?
With same USB cable ?
If remove your external wires, then working?
2024-01-30 08:03 AM - edited 2024-07-09 05:40 AM
@yugi wrote:no st link found error
I have attached the pic please give the solution .
Is the ST-Link being detected by the host computer?
eg, does the Virtual COM Port appear in the Device Manager?
If the host computer isn't detecting the ST-Link, then there's no way that any other app (eg, debugger or programmer) is going to be able to use it.
#STLinkVCP #STLinkComPort #DeviceManager
2024-01-30 10:40 PM
i'm check the stlink in device manager is showing the stlink
2024-01-31 01:26 AM - edited 2024-01-31 01:27 AM
Show a screenshot of the message(s) you receive
BTW: you can just paste an image into the post (as I did above) - no need to attach.