cancel
Showing results for 
Search instead for 
Did you mean: 

Problems getting the CAN transciever on STM32F769I-EVAL Board running

MH.6
Associate

I want to use the STM32F769I-EVAL Board to monitor a CAN netork. I configured the CAN module as it has been shown in the CAN_Loopback and in the CAN_Networking example.

The Loopback Example does run on my eval-board. I take that as confirmation, that I set up the CAN module the richt way. However the loopback mode does not use the transciever chip because the TX Signal is directly send back on the RX Line. I tested all possible jumper combinations with JP14, JP18 and JP19. Has anyone suggestions how to get the transciever working?

1 REPLY 1
Karl Yamashita
Lead III

if you want to use the CAN_Loopback example to use the CAN transceiver, then you need to modify the mode to

CanHandle.Init.Mode = CAN_MODE_NORMAL;

If smoke escapes your device, put the smoke back in. It'll still work as a conversation piece. If you find my answers useful, click the Accept as Solution button so that way others can see the solution.