2022-07-12 9:59 PM
Hi,
I created my new project follow the SubGHz Phy Ping Pong project. I want to write ADC values to FLASH for 5ms then enter stop 2 mode for 1000ms. In PWR_EnterStopMode() function, the HAL_SuspendTick() funciton is called, but my project enter stop 2 mode and exit stop 2 mode imediately. What wrong ?
I confused how to use sequencer correctly.
Please recommend me how to fix this problem.
My code below,
void PWR_EnterStopMode(void)
{
/* USER CODE BEGIN EnterStopMode_1 */
/* Disable ADC */
HAL_ADC_DeInit(&hadc);
/* Disable ADC voltage regulator */
HAL_ADCEx_DisableVoltageRegulator(&hadc);
/* USER CODE END EnterStopMode_1 */
HAL_SuspendTick();
/* Clear Status Flag before entering STOP/STANDBY Mode */
LL_PWR_ClearFlag_C1STOP_C1STB();
/* USER CODE BEGIN EnterStopMode_2 */
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 2000, RTC_WAKEUPCLOCK_RTCCLK_DIV16, 0);
/* USER CODE END EnterStopMode_2 */
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
/* USER CODE BEGIN EnterStopMode_3 */
/* USER CODE END EnterStopMode_3 */
}
Thanks.