cancel
Showing results for 
Search instead for 
Did you mean: 

problem with STM32_MAT-TARGET in external mode

sanjeevkumar TM
Associate II
Posted on January 19, 2018 at 07:41

hello i am using STM32_Mat_target 4.4.2 but i am not able to communicate my board stm32f407vg externally i am getting error for connection any one please help me regarding this

9 REPLIES 9
Posted on January 19, 2018 at 09:35

You mean this: 

http://www.st.com/en/development-tools/stm32-mat-target.html

  ?

You need to give more details about the 'error' you are receiving.

What basic connectivity checks have you done? eg, check in Device Manager ... ?

Is there no troubleshooting guidance in the documentation on the linked page?

sanjeevkumar TM
Associate II
Posted on January 19, 2018 at 11:20

I checked device manager also all connections are fine.. same external mode is working with embedded coder support package for stm32f4 discovery bord hardware support package.

But in that package PWM, SPI, I2C, UART blocks are not available.

Only ADC, and Digital i/p, o/p blocks with hardware interrupt blocks are there.

For my Research project almost all are required for analysis i need external mode.

Posted on January 19, 2018 at 11:15

Here i attach the error am getting and i followed the step as per the manual. can u please suggest me what exactly happening. also please tell a configuration required for this. her i attached configuration of cubemx also. you help is more appreciated. 

Thankyou

0690X00000609RAQAY.png0690X00000609HNQAY.png
Posted on January 19, 2018 at 12:33

The error message gives you 3 possible causes for the problem - have you checked each one?

Please give full details.

Posted on January 19, 2018 at 15:23

Thanks for your response. Also i resolved this issue

On Fri, Jan 19, 2018 at 5:05 PM, Andrew Neil <st-microelectronics@jiveon.com

Posted on January 19, 2018 at 16:10

For the benefit of future readers with the same problem, please describe how you resolved the issue.

Posted on February 01, 2018 at 10:04

Did you can resolved the problem?

Posted on February 02, 2018 at 05:35

sorry for the delay... I resolved but also have some other doubts regarding

the configuration of ADC in Cubemx.

1. Whatever the program I write it in Matlab after build into a Keil it

works fine in Keil software. But the result is not able to monitor in

Matlab.

2. Now I resolved this by enabling DMA in Cubemx. If we don't enable

this DMA we get only one conversion value in Matlan scope after it will not

show the conversion. But the conversion we can sea in Keil.

3. So, I have doubt on this configuration in Cubemx. Please help me

regarding this what configuration i have to do exactly in Cubemx

4. Last am not able to make out Single, continuous and discontinuous

conversion difference and how to set the delay in Matlab to read the ADC

value. now am not able to set a delay in this.

On Thu, Feb 1, 2018 at 2:36 PM, Aimagin Co., Ltd. <

Posted on February 09, 2018 at 11:44

Hi, Sanjeevkumar

I replied for the same problem in this

https://community.st.com/0D70X000006T0sJSAS

.

I hope it will be helpful to you.

Best regards,