2018-06-08 12:13 PM
The problem found in STM32 Cube MX 4.26.0, is that the tool over-wrote the
files of my project..I'll describe what happened:1. My project I was working on was created with STM32 Cube MX 4.25.0..2. I updated the STM32CubeMX.When opening my project, and make some changes and then asked togenerate the source code.A The first error message appears. Saying that there is a problem in theMakefileproject file.The following is an image with the error message.4. Changing the project settings, clicking the OK button displays the message
saying that my project already exists. And ask if I want to write over with anew project.The following is an image of STM Cube MX with error message [1]. We alsohave the file structure of my project [2].5. Clicking the ''No'' option, I can not implement my new settings.
By clicking the ''Yes'' option, the STM32 Cube MX overwrites the articles witha new project. In the following image shows the file structure of my project,it is important to note that some files have been removed from myproject.2018-06-09 3:12 PM
Hello
Teixeira.Evandro
,Can you please share your ioc or log file ?
We will raise this issue internally for check and come back to you soon.
With Regards,
Imen
2018-06-11 2:11 PM
Hello
DAHMEN.IMEN
,I do not have the .ioc file.Where the problem occurred.
I restored the project. And I went back to using STM32CubeMX 4.0.
2018-06-12 2:26 PM
Hello
DAHMEN.IMEN
.I have the same problem. Sequencing :
1.Create a project 2.Minimally set up 3. Generate the code-> the code is successfully generated 4. We ask to generate again and get an error.In version 4.25, everything worked well.
https://bitbucket.org/Shabashkin93/bug_stm32cubemx/src/master/log_bug_.txt
2018-06-12 2:50 PM
Hello
DAHMEN.IMEN
,Follow the .ioc file details
#MicroXplorer Configuration settings - do not modify
File.Version=6 KeepUserPlacement=true Mcu.Family=STM32F4 Mcu.IP0=NVIC Mcu.IP1=RCC Mcu.IP2=SYS Mcu.IPNb=3 Mcu.Name=STM32F407V(E-G)Tx Mcu.Package=LQFP100 Mcu.Pin0=PH0-OSC_IN Mcu.Pin1=PH1-OSC_OUT Mcu.Pin2=PA0-WKUP Mcu.Pin3=PD12 Mcu.Pin4=PD13 Mcu.Pin5=PD14 Mcu.Pin6=PD15 Mcu.Pin7=PD0 Mcu.Pin8=VP_SYS_VS_Systick Mcu.PinsNb=9 Mcu.ThirdPartyNb=0 Mcu.UserConstants= Mcu.UserName=STM32F407VGTx MxCube.Version=4.0 MxDb.Version=DB.4.0.260 NVIC.BusFault_IRQn=true\:0\:0\:false\:false\:false\:true NVIC.DebugMonitor_IRQn=true\:0\:0\:false\:false\:false\:true NVIC.HardFault_IRQn=true\:0\:0\:false\:false\:false\:true NVIC.MemoryManagement_IRQn=true\:0\:0\:false\:false\:false\:true NVIC.NonMaskableInt_IRQn=true\:0\:0\:false\:false\:false\:true NVIC.PendSV_IRQn=true\:0\:0\:false\:false\:true\:true NVIC.PriorityGroup=NVIC_PRIORITYGROUP_0 NVIC.SVCall_IRQn=true\:0\:0\:false\:false\:false\:true NVIC.SysTick_IRQn=true\:0\:0\:false\:false\:true\:true NVIC.UsageFault_IRQn=true\:0\:0\:false\:false\:false\:true PA0-WKUP.GPIOParameters=GPIO_PuPd,GPIO_Label,GPIO_ModeDefaultEXTI PA0-WKUP.GPIO_Label=B1 [Blue PushButton] PA0-WKUP.GPIO_ModeDefaultEXTI=GPIO_MODE_IT_RISING_FALLING PA0-WKUP.GPIO_PuPd=GPIO_NOPULL PA0-WKUP.Locked=true PA0-WKUP.Signal=GPXTI0 PCC.Checker=false PCC.Line=STM32F407/417 PCC.MCU=STM32F407V(E-G)Tx PCC.PartNumber=STM32F407VGTx PCC.Seq0=0 PCC.Series=STM32F4 PCC.Temperature=25 PCC.Vdd=3.3 PD0.GPIOParameters=GPIO_Speed,GPIO_Label PD0.GPIO_Label=LED PD0.GPIO_Speed=GPIO_SPEED_FREQ_HIGH PD0.Locked=true PD0.Signal=GPIO_Output PDGPIOParameters=GPIO_Speed,GPIO_PuPd,GPIO_Label PDGPIO_Label=LD4 [Green Led] PDGPIO_PuPd=GPIO_NOPULL PDGPIO_Speed=GPIO_SPEED_FREQ_LOW PDLocked=true PDSignal=GPIO_Output PDGPIOParameters=GPIO_Speed,GPIO_PuPd,GPIO_Label PDGPIO_Label=LD3 [Orange Led] PDGPIO_PuPd=GPIO_NOPULL PDGPIO_Speed=GPIO_SPEED_FREQ_LOW PDLocked=true PDSignal=GPIO_Output PDGPIOParameters=GPIO_Speed,GPIO_PuPd,GPIO_Label PDGPIO_Label=LD5 [Red Led] PDGPIO_PuPd=GPIO_NOPULL PDGPIO_Speed=GPIO_SPEED_FREQ_LOW PDLocked=true PDSignal=GPIO_Output PDGPIOParameters=GPIO_Speed,GPIO_PuPd,GPIO_Label PDGPIO_Label=LD6 [Blue Led] PDGPIO_PuPd=GPIO_NOPULL PDGPIO_Speed=GPIO_SPEED_FREQ_LOW PDLocked=true PDSignal=GPIO_Output PH0-OSC_IN.Mode=HSE-External-Oscillator PH0-OSC_IN.Signal=RCC_OSC_IN PH1-OSC_OUT.Mode=HSE-External-Oscillator PH1-OSC_OUT.Signal=RCC_OSC_OUT PinOutPanel.RotationAngle=0 ProjectManager.AskForMigrate=true ProjectManager.BackupPrevious=false ProjectManager.CompilerOptimize=3 ProjectManager.ComputerToolchain=false ProjectManager.CoupleFile=true ProjectManager.CustomerFirmwarePackage= ProjectManager.DefaultFWLocation=true ProjectManager.DeletePrevious=true ProjectManager.DeviceId=STM32F407VGTx ProjectManager.FirmwarePackage=STM32Cube FW_F4 V1.0 ProjectManager.FreePins=false ProjectManager.HalAssertFull=true ProjectManager.HeapSize=0x200 ProjectManager.KeepUserCode=true ProjectManager.LastFirmware=true ProjectManager.LibraryCopy=1 ProjectManager.MainLocation=Src ProjectManager.PreviousToolchain= ProjectManager.ProjectBuild=false ProjectManager.ProjectFileName=Kernel_RR.ioc ProjectManager.ProjectName=Kernel_RR ProjectManager.StackSize=0x400 ProjectManager.TargetToolchain=Makefile ProjectManager.ToolChainLocation= ProjectManager.UnderRoot=false ProjectManager.functionlistsort=1-MX_GPIO_Init-GPIO-false-HAL-true,2-SystemClock_Config-RCC-false-HAL-false RCC.48MHZClocksFreq_Value=48000000 RCC.AHBFreq_Value=168000000 RCC.APB1CLKDivider=RCC_HCLK_DIV4 RCC.APB1Freq_Value=42000000 RCC.APB1TimFreq_Value=84000000 RCC.APB2CLKDivider=RCC_HCLK_DIV2 RCC.APB2Freq_Value=84000000 RCC.APB2TimFreq_Value=168000000 RCC.CortexFreq_Value=168000000 RCC.EthernetFreq_Value=168000000 RCC.FCLKCortexFreq_Value=168000000 RCC.FamilyName=M RCC.HCLKFreq_Value=168000000 RCC.HSE_VALUE=8000000 RCC.HSI_VALUE=16000000 RCC.I2SClocksFreq_Value=192000000 RCC.IPParameters=48MHZClocksFreq_Value,AHBFreq_Value,APB1CLKDivider,APB1Freq_Value,APB1TimFreq_Value,APB2CLKDivider,APB2Freq_Value,APB2TimFreq_Value,CortexFreq_Value,EthernetFreq_Value,FCLKCortexFreq_Value,FamilyName,HCLKFreq_Value,HSE_VALUE,HSI_VALUE,I2SClocksFreq_Value,LSE_VALUE,LSI_VALUE,MCO2PinFreq_Value,PLLCLKFreq_Value,PLLM,PLLN,PLLQ,PLLQCLKFreq_Value,PLLSourceVirtual,RTCFreq_Value,RTCHSEDivFreq_Value,SYSCLKFreq_VALUE,SYSCLKSource,VCOI2SOutputFreq_Value,VCOInputFreq_Value,VCOOutputFreq_Value,VcooutputI2S RCC.LSE_VALUE=32768 RCC.LSI_VALUE=32000 RCC.MCO2PinFreq_Value=168000000 RCC.PLLCLKFreq_Value=168000000 RCC.PLLM=4 RCC.PLLN=168 RCC.PLLQ=7 RCC.PLLQCLKFreq_Value=48000000 RCC.PLLSourceVirtual=RCC_PLLSOURCE_HSE RCC.RTCFreq_Value=32000 RCC.RTCHSEDivFreq_Value=4000000 RCC.SYSCLKFreq_VALUE=168000000 RCC.SYSCLKSource=RCC_SYSCLKSOURCE_PLLCLK RCC.VCOI2SOutputFreq_Value=384000000 RCC.VCOInputFreq_Value=2000000 RCC.VCOOutputFreq_Value=336000000 RCC.VcooutputI2S=192000000 SH.GPXTI0.0=GPIO_EXTI0 SH.GPXTI0.ConfNb=1 VP_SYS_VS_Systick.Mode=SysTick VP_SYS_VS_Systick.Signal=SYS_VS_Systick board=STM32F4DISCOVERY boardIOC=true2018-06-25 9:33 AM
Hi Evandro,
Thanks for reporting this issue, the regeneration of makefile will be fixed in a next release.
For the files overwriting it is a normal behavior as you created a 'new' project that is not aware of added user files.
2018-06-28 6:27 AM
OK!
on the overwritten files, a New Project was Not created.
I simply changed the project settings. Next, a source code was generated.2018-08-03 2:38 AM
The same problem:
How can I change peripheral driver from HAL to LL without project re-creation?